DMP UI Demo Stub#

API and Callbacks for the DMP UI Demo Stub Component.

This component provides stubs for the DynamicMultiprotocolDemoLight app. Use this component to satisfy compilation when the display driver is not used, primarily when the Dynamic Multiprotocol UI Demo Code component is not enabled.

API#

enum
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_UNCHANGED
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_UNCHANGED
}
#define
#define
#define
#define

API Documentation#

sl_dmp_ui_light_state_t#

sl_dmp_ui_light_state_t
Enumerator
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_UNCHANGED
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_UNCHANGED

sl_dmp_ui_display_zigbee_state#

#define sl_dmp_ui_display_zigbee_state

sl_dmp_ui_zigbee_permit_join#

#define sl_dmp_ui_zigbee_permit_join

sl_dmp_ui_light_off#

#define sl_dmp_ui_light_off

sl_dmp_ui_light_on#

#define sl_dmp_ui_light_on

sl_dmp_ui_update_direction#

#define sl_dmp_ui_update_direction

sl_dmp_ui_bluetooth_connected#

#define sl_dmp_ui_bluetooth_connected

sl_dmp_ui_set_ble_device_name#

#define sl_dmp_ui_set_ble_device_name

sl_dmp_ui_init#

#define sl_dmp_ui_init

sl_dmp_ui_display_help#

#define sl_dmp_ui_display_help

DMP_UI_DIRECTION_INVALID#

#define DMP_UI_DIRECTION_INVALID
Value:
0

DMP_UI_DIRECTION_BLUETOOTH#

#define DMP_UI_DIRECTION_BLUETOOTH
Value:
1

DMP_UI_DIRECTION_SWITCH#

#define DMP_UI_DIRECTION_SWITCH
Value:
2

DMP_UI_DIRECTION_ZIGBEE#

#define DMP_UI_DIRECTION_ZIGBEE
Value:
3

DmpUiLightDirection_t#

#define DmpUiLightDirection_t
Value:
uint8_t

sl_dmp_ui_set_light_direction#

#define sl_dmp_ui_set_light_direction

sl_dmp_ui_get_light_direction#

#define sl_dmp_ui_get_light_direction
Value:
(...)