Modules#
EmberAfCalendarDayScheduleEntryStruct
EmberAfCalendarSpecialDayStruct
Calendar Common#
API and Callbacks for the Calendar Common Component.
This component provides common utility functions that are used by the client and server of the Calendar Cluster.
API#
Get the calendar by calendar ID.
Get the calendar end time (UTC).
Set the calendar info.
Add a new entry corresponding to the PublishCalendar command. Tries to handle the new entry in the following method: 1) Try to apply new data to a matching existing entry. 2) Fields such as providerId, issuerEventId, and startTime, will be used. 3) Overwrite the oldest entry (one with smallest event ID) with new information.
Set calendar server season info.
Add calendar server season info.
Set day profile info.
Add day profile info.
Set calendar server week profile info.
Add calendar server week profile.
Updating special days information of the specified calendar. Assumes that the value of totalNumberOfSpecialDays will match up with the information passed in between specialDaysEntries and specialDaysEntriesLength.
Enumerations#
Variables#
Macros#
API Documentation#
emberAfPluginCalendarCommonGetCalendarById#
uint8_t emberAfPluginCalendarCommonGetCalendarById (uint32_t calendarId, uint32_t providerId)
Get the calendar by calendar ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | calendarId | Ver.: always |
| uint32_t | N/A | providerId | Ver.: always |
Returns
uint8_t Calender index
emberAfPluginCalendarCommonEndTimeUtc#
uint32_t emberAfPluginCalendarCommonEndTimeUtc (const EmberAfCalendarStruct * calendar)
Get the calendar end time (UTC).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberAfCalendarStruct * | N/A | calendar | pointer to the calendar struct Ver.: always |
Returns
uint32_t end UTC time in seconds
emberAfCalendarCommonSetCalInfo#
bool emberAfCalendarCommonSetCalInfo (uint8_t index, uint32_t providerId, uint32_t issuerEventId, uint32_t issuerCalendarId, uint32_t startTimeUtc, uint8_t calendarType, uint8_t * calendarName, uint8_t numberOfSeasons, uint8_t numberOfWeekProfiles, uint8_t numberOfDayProfiles)
Set the calendar info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint32_t | N/A | providerId | Ver.: always |
| uint32_t | N/A | issuerEventId | Ver.: always |
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint32_t | N/A | startTimeUtc | Ver.: always |
| uint8_t | N/A | calendarType | Ver.: always |
| uint8_t * | N/A | calendarName | Ver.: always |
| uint8_t | N/A | numberOfSeasons | Ver.: always |
| uint8_t | N/A | numberOfWeekProfiles | Ver.: always |
| uint8_t | N/A | numberOfDayProfiles | Ver.: always |
Returns
bool true if success
emberAfCalendarCommonAddCalInfo#
bool emberAfCalendarCommonAddCalInfo (uint32_t providerId, uint32_t issuerEventId, uint32_t issuerCalendarId, uint32_t startTimeUtc, uint8_t calendarType, uint8_t * calendarName, uint8_t numberOfSeasons, uint8_t numberOfWeekProfiles, uint8_t numberOfDayProfiles)
Add a new entry corresponding to the PublishCalendar command. Tries to handle the new entry in the following method: 1) Try to apply new data to a matching existing entry. 2) Fields such as providerId, issuerEventId, and startTime, will be used. 3) Overwrite the oldest entry (one with smallest event ID) with new information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | providerId | Ver.: always |
| uint32_t | N/A | issuerEventId | Ver.: always |
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint32_t | N/A | startTimeUtc | Ver.: always |
| uint8_t | N/A | calendarType | Ver.: always |
| uint8_t * | N/A | calendarName | Ver.: always |
| uint8_t | N/A | numberOfSeasons | Ver.: always |
| uint8_t | N/A | numberOfWeekProfiles | Ver.: always |
| uint8_t | N/A | numberOfDayProfiles | Ver.: always |
Returns
bool true if success
emberAfCalendarServerSetSeasonsInfo#
bool emberAfCalendarServerSetSeasonsInfo (uint8_t index, uint8_t seasonId, EmberAfDate startDate, uint8_t weekIndex)
Set calendar server season info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint8_t | N/A | seasonId | Ver.: always |
| EmberAfDate | N/A | startDate | Ver.: always |
| uint8_t | N/A | weekIndex | Ver.: always |
Returns
bool true if success
emberAfCalendarServerAddSeasonsInfo#
bool emberAfCalendarServerAddSeasonsInfo (uint32_t issuerCalendarId, uint8_t * seasonsEntries, uint8_t seasonsEntriesLength, uint8_t * unknownWeekIdSeasonsMask)
Add calendar server season info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint8_t * | N/A | seasonsEntries | Ver.: always |
| uint8_t | N/A | seasonsEntriesLength | Ver.: always |
| uint8_t * | N/A | unknownWeekIdSeasonsMask | Ver.: always |
Returns
bool true if success
emberAfCalendarCommonSetDayProfInfo#
bool emberAfCalendarCommonSetDayProfInfo (uint8_t index, uint8_t dayId, uint8_t entryId, uint16_t minutesFromMidnight, uint8_t data)
Set day profile info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint8_t | N/A | dayId | Ver.: always |
| uint8_t | N/A | entryId | Ver.: always |
| uint16_t | N/A | minutesFromMidnight | Ver.: always |
| uint8_t | N/A | data | Ver.: always |
Returns
bool true if success
emberAfCalendarCommonAddDayProfInfo#
bool emberAfCalendarCommonAddDayProfInfo (uint32_t issuerCalendarId, uint8_t dayId, uint8_t * dayScheduleEntries, uint16_t dayScheduleEntriesLength)
Add day profile info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint8_t | N/A | dayId | Ver.: always |
| uint8_t * | N/A | dayScheduleEntries | Ver.: always |
| uint16_t | N/A | dayScheduleEntriesLength | Ver.: always |
Returns
bool true if success
emberAfCalendarServerSetWeekProfInfo#
bool emberAfCalendarServerSetWeekProfInfo (uint8_t index, uint8_t weekId, uint8_t dayIdRefMon, uint8_t dayIdRefTue, uint8_t dayIdRefWed, uint8_t dayIdRefThu, uint8_t dayIdRefFri, uint8_t dayIdRefSat, uint8_t dayIdRefSun)
Set calendar server week profile info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint8_t | N/A | weekId | Ver.: always |
| uint8_t | N/A | dayIdRefMon | Ver.: always |
| uint8_t | N/A | dayIdRefTue | Ver.: always |
| uint8_t | N/A | dayIdRefWed | Ver.: always |
| uint8_t | N/A | dayIdRefThu | Ver.: always |
| uint8_t | N/A | dayIdRefFri | Ver.: always |
| uint8_t | N/A | dayIdRefSat | Ver.: always |
| uint8_t | N/A | dayIdRefSun | Ver.: always |
Returns
bool true if success
emberAfCalendarServerAddWeekProfInfo#
bool emberAfCalendarServerAddWeekProfInfo (uint32_t issuerCalendarId, uint8_t weekId, uint8_t dayIdRefMon, uint8_t dayIdRefTue, uint8_t dayIdRefWed, uint8_t dayIdRefThu, uint8_t dayIdRefFri, uint8_t dayIdRefSat, uint8_t dayIdRefSun)
Add calendar server week profile.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint8_t | N/A | weekId | Ver.: always |
| uint8_t | N/A | dayIdRefMon | Ver.: always |
| uint8_t | N/A | dayIdRefTue | Ver.: always |
| uint8_t | N/A | dayIdRefWed | Ver.: always |
| uint8_t | N/A | dayIdRefThu | Ver.: always |
| uint8_t | N/A | dayIdRefFri | Ver.: always |
| uint8_t | N/A | dayIdRefSat | Ver.: always |
| uint8_t | N/A | dayIdRefSun | Ver.: always |
Returns
bool true if success
emberAfCalendarCommonAddSpecialDaysInfo#
bool emberAfCalendarCommonAddSpecialDaysInfo (uint32_t issuerCalendarId, uint8_t totalNumberOfSpecialDays, uint8_t * specialDaysEntries, uint16_t specialDaysEntriesLength, uint8_t * unknownSpecialDaysMask)
Updating special days information of the specified calendar. Assumes that the value of totalNumberOfSpecialDays will match up with the information passed in between specialDaysEntries and specialDaysEntriesLength.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | issuerCalendarId | Ver.: always |
| uint8_t | N/A | totalNumberOfSpecialDays | Ver.: always |
| uint8_t * | N/A | specialDaysEntries | Ver.: always |
| uint16_t | N/A | specialDaysEntriesLength | Ver.: always |
| uint8_t * | N/A | unknownSpecialDaysMask | Ver.: always |
Returns
bool true if success
Enumeration Documentation#
EmberAfPluginCalendarCommonFlags#
EmberAfPluginCalendarCommonFlags
| Enumerator | |
|---|---|
| EMBER_AF_PLUGIN_CALENDAR_COMMON_FLAGS_SENT | |
Macro Definition Documentation#
EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_SCHEDULE_ENTRY#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_SCHEDULE_ENTRYValue:
0xFFFF
EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_ID#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_IDValue:
0xFF
EMBER_AF_PLUGIN_CALENDAR_MAX_CALENDAR_NAME_LENGTH#
#define EMBER_AF_PLUGIN_CALENDAR_MAX_CALENDAR_NAME_LENGTHValue:
12
EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_INDEX#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_INDEXValue:
0xFF
EMBER_AF_PLUGIN_CALENDAR_COMMON_MONDAY_INDEX#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_MONDAY_INDEXValue:
(0)
EMBER_AF_PLUGIN_CALENDAR_COMMON_SUNDAY_INDEX#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_SUNDAY_INDEXValue:
(6)
EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_CALENDAR_ID#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_INVALID_CALENDAR_IDValue:
0xFFFFFFFF
EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_CALENDAR_ID#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_CALENDAR_IDValue:
0x00000000
EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_PROVIDER_ID#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_PROVIDER_IDValue:
0xFFFFFFFF
EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_ISSUER_ID#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_ISSUER_IDValue:
0xFFFFFFFF
EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_CALENDAR_TYPE#
#define EMBER_AF_PLUGIN_CALENDAR_COMMON_WILDCARD_CALENDAR_TYPEValue:
0xFF