You are viewing documentation for version:
Data point descriptor. Compact attribute, Multi sensor or Generic switch feature uses this as descriptor to interpret the incoming data from the GPD. This descriptor is set up at the sink during the commissioning.
Public Attribute Documentation#
nbAttrRecord#
uint8_t EmberGpDataPointDescriptor::nbAttrRecord
Number of attribute records
clientServer#
uint8_t EmberGpDataPointDescriptor::clientServer
Client or Server flag
ManIdPresent#
uint8_t EmberGpDataPointDescriptor::ManIdPresent
Manufacture ID present
datapointOptions#
uint8_t EmberGpDataPointDescriptor::datapointOptions
Data point options
clusterID#
uint16_t EmberGpDataPointDescriptor::clusterID
Cluster ID
manufacturerID#
uint16_t EmberGpDataPointDescriptor::manufacturerID
Manufacture ID
attrRecord#
EmberGpAttributeRecord EmberGpDataPointDescriptor::attrRecord
Attribute Record