The internal representation of a sink table entry.
Public Attribute Documentation#
status#
EmberGpSinkTableEntryStatus EmberGpSinkTableEntry::status
Internal status. Defines if the entry is unused or used as a sink table entry
options#
uint16_t EmberGpSinkTableEntry::options
The tunneling options (this contains both options and extendedOptions from the spec)
sinkList#
EmberGpSinkListEntry EmberGpSinkTableEntry::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks; hardcoded to 2, which is the spec minimum
gpdSecurityFrameCounter#
EmberGpSecurityFrameCounter EmberGpSinkTableEntry::gpdSecurityFrameCounter
The SFC of the GPD