You are viewing documentation for version:
Generic Switch Information. Generic switch feature uses this as descriptor to interpret the incoming switch command from the GPD. This information is set up at the sink during the commissioning. 
Public Attribute Documentation#
switchInfoLength#
uint8_t EmberGpSwitchInformation::switchInfoLength
Switch Information Length 
nbOfContacts#
uint8_t EmberGpSwitchInformation::nbOfContacts
Number of contacts in the switch 
switchType#
uint8_t EmberGpSwitchInformation::switchType
Switch type 
currentContact#
uint8_t EmberGpSwitchInformation::currentContact
Current contact 
savedContact#
uint8_t EmberGpSwitchInformation::savedContact
Saved contacts