GP Tx queue entry.

Public Attribute Documentation#

inUse#

bool EmberGpTxQueueEntry::inUse

The entry in use


useCca#

bool EmberGpTxQueueEntry::useCca

Use CCA during transmit


addr#

EmberGpAddress EmberGpTxQueueEntry::addr

GP address


gpdCommandId#

uint8_t EmberGpTxQueueEntry::gpdCommandId

GPD Command ID


asdu#

EmberMessageBuffer EmberGpTxQueueEntry::asdu

Buffer holding ASDU


gpepHandle#

uint8_t EmberGpTxQueueEntry::gpepHandle

Handle for the outgoing message


queueEntryLifetimeMs#

uint16_t EmberGpTxQueueEntry::queueEntryLifetimeMs

Life time in milliseconds for the entry to expire, 0 indicates no expiry