Cluster Commands: Poll Control#

This group describes the CLI commands for the Poll Control cluster. Listed below is a description of the cluster:

This cluster provides a mechanism for the management of an end device's MAC Data Poll rate. For the purposes of this cluster, the term "poll" always refers to the sending of a MAC Data Poll from the end device to the end device's parent.

Macros#

#define

zcl poll-control long [newLongPollInterval:4]

#define

zcl poll-control short [newShortPollInterval:2]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_STOP

zcl poll-control stop

  • The Fast Poll Stop command is used to stop the fast poll mode initiated by the Check-in response.


Definition at line 1523 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_LONG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_LONG

zcl poll-control long [newLongPollInterval:4]

  • The Set Long Poll Interval command is used to set the read only Long Poll Interval Attribute.

    • newLongPollInterval - INT32U


Definition at line 1529 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_SHORT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_POLL_CONTROL_SHORT

zcl poll-control short [newShortPollInterval:2]

  • The Set Short Poll Interval command is used to set the read only Short Poll Interval Attribute.

    • newShortPollInterval - INT16U


Definition at line 1535 of file app/framework/test/headers/cli.doc