Application Framework Types#
This documentation describes the types used by the Zigbee Application Framework.
Modules#
EmberAfDefaultOrMinMaxAttributeValue
EmberAfPluginMessagingClientMessage
EmberAfPluginZllCommissioningGroupInformationRecord
EmberAfPluginZllCommissioningEndpointInformationRecord
EmberAfImageBlockRequestCallbackStruct
EmberAfStandaloneBootloaderQueryResponseData
EmberAfDeviceManagementTenancy
EmberAfDeviceManagementSupplier
EmberAfDeviceManagementSupplyStatusFlags
EmberAfDeviceManagementUncontrolledFlowThreshold
EmberAfDeviceManagementSupplyStatus
EmberAfDeviceManagementPassword
EmberAfDeviceManagementAttributeRange
EmberAfDeviceManagementAttributeTable
Enumerations#
Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.
Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.
Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.
Specifies CPP Authorization values.
Status codes used by the ZLL Commissioning plugin.
The list of options possible for the image block request/response.
Contain the success or error code of an OTA storage device operation.
Contain the success or error code of an OTA download operation.
Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.
CBKE Library types.
Typedefs#
Refer to the Zigbee application profile ID.
Refer to the ZCL attribute ID.
Refer to the ZCL cluster ID.
Refer to the ZCL attribute type.
User for the cluster mask.
User for the attribute mask.
Use for either of the cluster functions.
Interpan Message type: unicast, broadcast, or multicast.
The options for sending/receiving interpan messages.
The options for what interpan messages are allowed.
Bitmask data type for storing one bit of information for each ESI in the ESI table.
Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
Refer to the handler for network events.
Refer to the handler for endpoint events.
Refer to the tick callback for cluster.
Refer to the init callback for cluster.
Refer to the attribute changed callback function.
Refer to the manufacturer-specific attribute changed callback function.
Refer to the pre-attribute changed callback function.
Refer to the default response callback function.
Refer to the message sent callback function.
Zigbee Internet Client/Server Remote Cluster Types.
Macros#
A distinguished manufacturer code that is used to indicate the absence of a manufacturer-specific profile, cluster, command, or attribute.
An invalid profile ID This is a reserved profileId.
A simple way to determine if the service discovery callback has a response.
Indicate the absence of a Group table entry.
Value used when setting or getting the endpoint in a Group table entry. It indicates that the entry is not in use.
Maximum length of Group names, not including the length byte.
Indicates the absence of a Scene table entry.
Value used when setting or getting the endpoint in a Scene table entry. It indicates that the entry is not in use.
Maximum length of Scene names, not including the length byte.
The group identifier for the global scene.
The scene identifier for the global scene.
Use when setting or getting the endpoint in a report table entry. It indicates that the entry is not in use.
The maximum size of the string that is present in the header of the Zigbee Over-the-air file format.
The length of the hardware tag in the Ember Bootloader Query Response.
Device Management plugin types.
Permit join times.
The overhead of the ZDO response. 1 byte for the sequence and 1 byte for the status code.
Enumeration Documentation#
EmberAfSecurityProfile#
EmberAfSecurityProfile
| Enumerator | |
|---|---|
| EMBER_AF_SECURITY_PROFILE_NONE | |
| EMBER_AF_SECURITY_PROFILE_HA | |
| EMBER_AF_SECURITY_PROFILE_HA12 | |
| EMBER_AF_SECURITY_PROFILE_SE_TEST | |
| EMBER_AF_SECURITY_PROFILE_SE_FULL | |
| EMBER_AF_SECURITY_PROFILE_Z3 | |
| EMBER_AF_SECURITY_PROFILE_CUSTOM | |
EmberAfServiceDiscoveryStatus#
EmberAfServiceDiscoveryStatus
Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
| Enumerator | |
|---|---|
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
EmberAfEventPollControl#
EmberAfEventPollControl
Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.
| Enumerator | |
|---|---|
| EMBER_AF_LONG_POLL | |
| EMBER_AF_SHORT_POLL | |
EmberAfEventSleepControl#
EmberAfEventSleepControl
Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.
| Enumerator | |
|---|---|
| EMBER_AF_OK_TO_SLEEP | |
| EMBER_AF_OK_TO_HIBERNATE | Deprecated |
| EMBER_AF_OK_TO_NAP | Deprecated |
| EMBER_AF_STAY_AWAKE | |
EmberAfApplicationTask#
EmberAfApplicationTask
Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.
Some tasks do not necessarily have a response. For example, a ZDO request may or may not have a response. In this case, the application framework cannot rely on the fact that a response will come in to end the wake cycle, so the Application framework must time out the wake cycle if no expected response is received or no other event can be relied upon to end the wake cycle.
Add these types of tasks to the wake timeout mask by calling emberAfSetWakeTimeoutBitmaskCallback so that they can be governed by a timeout instead of a request / response.
The current tasks bitmask is an uint32_t bitmask used to track which tasks are active at any given time. The bottom 16 bits, values 0x01 - 0x8000 are reserved for Ember's use. The top 16 bits are reserved for the customer, values 0x10000 - 0x80000000
| Enumerator | |
|---|---|
| EMBER_AF_WAITING_FOR_DATA_ACK | |
| EMBER_AF_LAST_POLL_GOT_DATA | |
| EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY | |
| EMBER_AF_WAITING_FOR_ZDO_RESPONSE | |
| EMBER_AF_WAITING_FOR_ZCL_RESPONSE | |
| EMBER_AF_WAITING_FOR_REGISTRATION | |
| EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE | |
| EMBER_AF_FORCE_SHORT_POLL | |
| EMBER_AF_FRAGMENTATION_IN_PROGRESS | |
| EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY | |
| EMBER_AF_WAITING_FOR_TC_KEY_UPDATE | |
EmberAfPluginPriceCppAuth#
EmberAfPluginPriceCppAuth
Specifies CPP Authorization values.
| Enumerator | |
|---|---|
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED | |
EmberAfPluginTunnelingClientStatus#
EmberAfPluginTunnelingClientStatus
| Enumerator | |
|---|---|
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT | |
EmberAfZllCommissioningStatus#
EmberAfZllCommissioningStatus
Status codes used by the ZLL Commissioning plugin.
| Enumerator | |
|---|---|
| EMBER_AF_ZLL_ABORTED_BY_APPLICATION | |
| EMBER_AF_ZLL_CHANNEL_CHANGE_FAILED | |
| EMBER_AF_ZLL_JOINING_FAILED | |
| EMBER_AF_ZLL_NO_NETWORKS_FOUND | |
| EMBER_AF_ZLL_PREEMPTED_BY_STACK | |
| EMBER_AF_ZLL_SENDING_START_JOIN_FAILED | |
| EMBER_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED | |
| EMBER_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED | |
| EMBER_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED | |
| EMBER_AF_ZLL_NETWORK_FORMATION_FAILED | |
| EMBER_AF_ZLL_NETWORK_UPDATE_OPERATION | |
EmberAfImageBlockRequestOptions#
EmberAfImageBlockRequestOptions
The list of options possible for the image block request/response.
| Enumerator | |
|---|---|
| EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST | |
EmberAfOtaStorageStatus#
EmberAfOtaStorageStatus
Contain the success or error code of an OTA storage device operation.
| Enumerator | |
|---|---|
| EMBER_AF_OTA_STORAGE_SUCCESS | |
| EMBER_AF_OTA_STORAGE_ERROR | |
| EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG | |
| EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND | |
| EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS | |
EmberAfOtaDownloadResult#
EmberAfOtaDownloadResult
Contain the success or error code of an OTA download operation.
| Enumerator | |
|---|---|
| EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS | |
| EMBER_AF_OTA_DOWNLOAD_TIME_OUT | |
| EMBER_AF_OTA_VERIFY_FAILED | |
| EMBER_AF_OTA_SERVER_ABORTED | |
| EMBER_AF_OTA_CLIENT_ABORTED | |
| EMBER_AF_OTA_ERASE_FAILED | |
EmberAfKeyEstablishmentNotifyMessage#
EmberAfKeyEstablishmentNotifyMessage
| Enumerator | |
|---|---|
| NO_APP_MESSAGE | |
| RECEIVED_PARTNER_CERTIFICATE | |
| GENERATING_EPHEMERAL_KEYS | |
| GENERATING_SHARED_SECRET | |
| KEY_GENERATION_DONE | |
| GENERATE_SHARED_SECRET_DONE | |
| LINK_KEY_ESTABLISHED | LINK_KEY_ESTABLISHED indicates Success, key establishment done. |
| NO_LOCAL_RESOURCES | Error codes: Transient failures where Key Establishment could be retried. |
| PARTNER_NO_RESOURCES | |
| TIMEOUT_OCCURRED | |
| INVALID_APP_COMMAND | |
| MESSAGE_SEND_FAILURE | |
| PARTNER_SENT_TERMINATE | |
| INVALID_PARTNER_MESSAGE | |
| PARTNER_SENT_DEFAULT_RESPONSE_ERROR | |
| BAD_CERTIFICATE_ISSUER | Fatal Errors: These results are not worth retrying because the outcome will not change. |
| KEY_CONFIRM_FAILURE | |
| BAD_KEY_ESTABLISHMENT_SUITE | |
| KEY_TABLE_FULL | |
| NO_ESTABLISHMENT_ALLOWED | Neither initiator nor responder is an ESP/TC so the key establishment is not allowed per the spec. |
| INVALID_CERTIFICATE_KEY_USAGE | |
EmberAfImageVerifyStatus#
EmberAfImageVerifyStatus
Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.
| Enumerator | |
|---|---|
| EMBER_AF_IMAGE_GOOD | |
| EMBER_AF_IMAGE_BAD | |
| EMBER_AF_IMAGE_VERIFY_IN_PROGRESS | |
EmberAfCbkeKeyEstablishmentSuite#
EmberAfCbkeKeyEstablishmentSuite
CBKE Library types.
| Enumerator | |
|---|---|
| EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE | |
| EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 | |
| EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 | |
EmberAfDeviceManagementPasswordType#
EmberAfDeviceManagementPasswordType
| Enumerator | |
|---|---|
| UNUSED_PASSWORD | |
| SERVICE_PASSWORD | |
| CONSUMER_PASSWORD | |
EmberAfDeviceManagementChangePendingFlags#
EmberAfDeviceManagementChangePendingFlags
| Enumerator | |
|---|---|
| EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK | |
EmberAfDeviceDiscoveryStatus#
EmberAfDeviceDiscoveryStatus
| Enumerator | |
|---|---|
| EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED | |
Typedef Documentation#
EmberAfGenericClusterFunction#
typedef void(* EmberAfGenericClusterFunction) (void) )(void)
Use for either of the cluster functions.
This type is used for the array of the cluster functions and should always be cast into one of the specific functions before being called.
EmberAfDifferenceType#
typedef uint64_t EmberAfDifferenceType
Compare two ZCL attribute values. The size of this data type depends on the platform.
EmberAfInterpanMessageType#
typedef uint8_t EmberAfInterpanMessageType
Interpan Message type: unicast, broadcast, or multicast.
EmberAfInterpanOptions#
typedef uint16_t EmberAfInterpanOptions
The options for sending/receiving interpan messages.
EmberAfAllowedInterpanOptions#
typedef uint8_t EmberAfAllowedInterpanOptions
The options for what interpan messages are allowed.
EmberAfPluginEsiManagementBitmask#
typedef uint8_t EmberAfPluginEsiManagementBitmask
Bitmask data type for storing one bit of information for each ESI in the ESI table.
EmberAfServiceDiscoveryCallback#
typedef void() EmberAfServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult *result) (const EmberAfServiceDiscoveryResult *result)
Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
EmberAfPartnerLinkKeyExchangeCallback#
typedef void() EmberAfPartnerLinkKeyExchangeCallback(bool success) (bool success)
Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
EmberAfNetworkEventHandler#
typedef void(* EmberAfNetworkEventHandler) (void) )(void)
Refer to the handler for network events.
EmberAfEndpointEventHandler#
typedef void(* EmberAfEndpointEventHandler) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the handler for endpoint events.
EmberAfTickFunction#
typedef void(* EmberAfTickFunction) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the tick callback for cluster.
Tick function will be called once for each tick for each endpoint in the cluster. The rate of tick is determined by the metadata of the cluster.
EmberAfInitFunction#
typedef void(* EmberAfInitFunction) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the init callback for cluster.
Init function is called when the application starts up, once for each cluster/endpoint combination.
EmberAfClusterAttributeChangedCallback#
typedef void(* EmberAfClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId) )(uint8_t endpoint, EmberAfAttributeId attributeId)
Refer to the attribute changed callback function.
This function is called just after an attribute changes.
EmberAfManufacturerSpecificClusterAttributeChangedCallback#
typedef void(* EmberAfManufacturerSpecificClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode) )(uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode)
Refer to the manufacturer-specific attribute changed callback function.
This function is called just after a manufacturer-specific attribute changes.
EmberAfClusterPreAttributeChangedCallback#
typedef EmberAfStatus(* EmberAfClusterPreAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value) )(uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value)
Refer to the pre-attribute changed callback function.
This function is called before an attribute changes.
EmberAfDefaultResponseFunction#
typedef void(* EmberAfDefaultResponseFunction) (uint8_t endpoint, uint8_t commandId, EmberAfStatus status) )(uint8_t endpoint, uint8_t commandId, EmberAfStatus status)
Refer to the default response callback function.
This function is called when default response is received, before the global callback. Global callback is called immediately afterwards.
EmberAfMessageSentFunction#
typedef void(* EmberAfMessageSentFunction) (EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status) )(EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status)
Refer to the message sent callback function.
This function is called when a message is sent.
EmberAfRemoteClusterType#
typedef uint16_t EmberAfRemoteClusterType
Zigbee Internet Client/Server Remote Cluster Types.