EZ Mode#
Callbacks for EZ Mode Component.
Callbacks#
void
sl_zigbee_af_ezmode_commissioning_client_complete_cb(uint8_t bindingIndex)
Client complete.
Callbacks Documentation#
sl_zigbee_af_ezmode_commissioning_client_complete_cb#
void sl_zigbee_af_ezmode_commissioning_client_complete_cb (uint8_t bindingIndex)
Client complete.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | bindingIndex | The binding index that was created or ::SL_ZIGBEE_NULL_BINDING if an error occurred. Ver.: always |
This function is called by the EZ Mode Commissioning plugin when client commissioning completes.