Public Attribute Documentation#

allocateMemoryForResponses#

bool sl_zigbee_af_gbz_message_creator_state_t::allocateMemoryForResponses

Definition at line 175 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

command#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::command

Definition at line 178 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

commandIndex#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::commandIndex

Definition at line 179 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

commandLength#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::commandLength

Definition at line 180 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

responses#

sli_zigbee_af_gbz_use_case_specific_component* sl_zigbee_af_gbz_message_creator_state_t::responses

Definition at line 183 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

lastResponse#

sli_zigbee_af_gbz_use_case_specific_component* sl_zigbee_af_gbz_message_creator_state_t::lastResponse

Definition at line 184 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

header#

sli_zigbee_af_gbz_payload_header* sl_zigbee_af_gbz_message_creator_state_t::header

Definition at line 185 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextEncryptedComponentZclSequenceNumber#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextEncryptedComponentZclSequenceNumber

Definition at line 188 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextComponentZclSequenceNumber#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextComponentZclSequenceNumber

Definition at line 189 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextAdditionalHeaderFrameCounter#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextAdditionalHeaderFrameCounter

Definition at line 190 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

componentsCount#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::componentsCount

Definition at line 191 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

lastExtHeaderControlField#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::lastExtHeaderControlField

Definition at line 192 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

messageCode#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::messageCode

Definition at line 193 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

result#

sl_zigbee_af_gbz_message_creator_result_t sl_zigbee_af_gbz_message_creator_state_t::result

Definition at line 196 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h