The internal representation of a sink table entry.

Public Attribute Documentation#

status#

sl_zigbee_gp_sink_table_entry_status_t sl_zigbee_gp_sink_table_entry_t::status

Internal status. Defines if the entry is unused or used as a sink table entry


options#

uint16_t sl_zigbee_gp_sink_table_entry_t::options

The tunneling options (this contains both options and extendedOptions from the spec)


gpd#

sl_zigbee_gp_address_t sl_zigbee_gp_sink_table_entry_t::gpd

The addressing info of the GPD


deviceId#

uint8_t sl_zigbee_gp_sink_table_entry_t::deviceId

The device ID for the GPD


sinkList#

sl_zigbee_gp_sink_list_entry_t sl_zigbee_gp_sink_table_entry_t::sinkList[GP_SINK_LIST_ENTRIES]

The list of sinks; hardcoded to 2, which is the spec minimum


assignedAlias#

sl_802154_short_addr_t sl_zigbee_gp_sink_table_entry_t::assignedAlias

The assigned alias for the GPD


groupcastRadius#

uint8_t sl_zigbee_gp_sink_table_entry_t::groupcastRadius

The groupcast radius


securityOptions#

uint8_t sl_zigbee_gp_sink_table_entry_t::securityOptions

The security options field


gpdSecurityFrameCounter#

sl_zigbee_gp_security_frame_counter_t sl_zigbee_gp_sink_table_entry_t::gpdSecurityFrameCounter

The SFC of the GPD


gpdKey#

sl_zigbee_key_data_t sl_zigbee_gp_sink_table_entry_t::gpdKey

The GPD key associated with this entry.