Generic Switch Information. Generic switch feature uses this as descriptor to interpret the incoming switch command from the GPD. This information is set up at the sink during the commissioning.

Public Attributes#

uint8_t

Public Attribute Documentation#

switchInfoLength#

uint8_t sl_zigbee_gp_switch_information_t::switchInfoLength

Switch Information Length


Definition at line 688 of file stack/include/gp-types.h

nbOfContacts#

uint8_t sl_zigbee_gp_switch_information_t::nbOfContacts

Number of contacts in the switch


Definition at line 690 of file stack/include/gp-types.h

switchType#

uint8_t sl_zigbee_gp_switch_information_t::switchType

Switch type


Definition at line 692 of file stack/include/gp-types.h

currentContact#

uint8_t sl_zigbee_gp_switch_information_t::currentContact

Current contact


Definition at line 694 of file stack/include/gp-types.h

savedContact#

uint8_t sl_zigbee_gp_switch_information_t::savedContact

Saved contacts


Definition at line 696 of file stack/include/gp-types.h