Information discovered during a ZLL scan about the ZLL device's endpoint information.

Public Attributes#

sl_802154_long_addr_t
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

ieeeAddress#

sl_802154_long_addr_t sl_zigbee_zll_device_info_record_t::ieeeAddress

Definition at line 153 of file stack/include/zll-types.h

endpointId#

uint8_t sl_zigbee_zll_device_info_record_t::endpointId

Definition at line 154 of file stack/include/zll-types.h

profileId#

uint16_t sl_zigbee_zll_device_info_record_t::profileId

Definition at line 155 of file stack/include/zll-types.h

deviceId#

uint16_t sl_zigbee_zll_device_info_record_t::deviceId

Definition at line 156 of file stack/include/zll-types.h

version#

uint8_t sl_zigbee_zll_device_info_record_t::version

Definition at line 157 of file stack/include/zll-types.h

groupIdCount#

uint8_t sl_zigbee_zll_device_info_record_t::groupIdCount

Definition at line 158 of file stack/include/zll-types.h