Delayed Join#

API and Callbacks for the Delayed Join Component.

This component is used both for a trust center and a joining device. It provides a set of APIs for setting the acceptable delay for receiving a network key, as well as sending the network key on demand from the app. The following are the minimum conditions to verify before successfully using this component:

  • 1.The trust center must have an acceptable version of a link key for the joining devices.

  • 2.The component must be (re-)activated every time a network is opened or after any other event that changes the trust center (re-)join policy.

API#

void

Set the network timeout value.

void

Set the activation state of Delayed Join component.

bool

Return true if the TC is delaying in sending the network key to newly joining devices.

Macros#

#define
SL_ZIGBEE_AF_PLUGIN_DELAYED_JOIN_PLUGIN_NAME "Delayed Join"
#define
SL_ZIGBEE_AF_PLUGIN_DELAYED_JOIN_MAXIMUM_TIMEOUT_SUPPORTED_S 65

API Documentation#

sl_zigbee_af_delayed_join_set_network_key_timeout#

void sl_zigbee_af_delayed_join_set_network_key_timeout (uint8_t timeout)

Set the network timeout value.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Atimeout

timeout value. Acceptable range 3-255 Ver.: always


sl_zigbee_af_delayed_join_activate#

void sl_zigbee_af_delayed_join_activate (bool activated)

Set the activation state of Delayed Join component.

Parameters
TypeDirectionArgument NameDescription
boolN/Aactivated

Indicates whether to activate the Delayed Join functionality


sl_zigbee_af_delayed_join_is_activated#

bool sl_zigbee_af_delayed_join_is_activated (void )

Return true if the TC is delaying in sending the network key to newly joining devices.

Parameters
TypeDirectionArgument NameDescription
voidN/A