Device Table#

API and Callbacks for the Device Table Component.

Simple C-based rules engine for demonstrating automatic control through a gateway.

Modules#

sl_zigbee_af_plugin_device_table_entry_t

API#

void

Send a message using the device table.

void
sl_zigbee_af_device_table_send(sl_802154_long_addr_t eui64, uint8_t endpoint)

Send a message using the device table.

void

Send a CLI command based on an index and an endpoint.

void

Send an internally-generated command.

void
sl_zigbee_af_device_table_command_send_with_endpoint(sl_802154_long_addr_t eui64, uint8_t endpoint)

Send an internally-generated command.

void

Send an internally-generated command.

bool
sl_zigbee_af_device_table_get_eui64_from_node_id(sl_802154_short_addr_t sl_zigbee_node_id, sl_802154_long_addr_t eui64)

Compute the EUI64 from the node ID in the device table.

uint16_t

Compute the node ID from the device table index.

uint16_t
sl_zigbee_af_device_table_get_endpoint_from_node_id_and_endpoint(sl_802154_short_addr_t sl_zigbee_node_id, uint8_t endpoint)

Find the endpoint index from node ID and endpoint number.

uint16_t
sl_zigbee_af_device_table_get_index_from_node_id(sl_802154_short_addr_t sl_zigbee_node_id)

Find the index based on the node ID.

uint16_t

Find the index based on the EUI64.

uint16_t
sl_zigbee_af_device_table_get_index_from_eui64_and_endpoint(sl_802154_long_addr_t eui64, uint8_t endpoint)

Find the index based on the EUI64 and endpoint.

uint16_t

Find the node ID based on the EUI64.

void
sl_zigbee_af_device_table_message_sent_status(sl_802154_short_addr_t nodeId, sl_status_t status, uint16_t profileId, uint16_t clusterId)

Change the device status based on the last sent message.

void

Send a leave message to a device based on the index.

void
sl_zigbee_af_device_table_message_received(sl_802154_short_addr_t nodeId)

Inform the device table that a message was received.

void

Kick off device table route repair.

Return a pointer to the device table structure.

Return a pointer to the device table entry.

void
sl_zigbee_af_device_table_new_device_join_handler(sl_802154_short_addr_t newNodeId, sl_802154_long_addr_t newNodeEui64)

Inform the device table that a new device joined.

uint32_t

Calculate time since the device heard the last message.

bool
sl_zigbee_af_device_table_match_eui64(sl_802154_long_addr_t a, sl_802154_long_addr_t b)

Return true if the two EUI64 parameters match.

void

Clear the device table.

void

Called when a device has been removed from the device table.

void

Called when the device table has been initialized.

Enumerations#

enum
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_NULL = 0x00
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_JOINED = 0x10
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_UNRESPONSIVE = 0x11
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_LEAVE_SENT = 0x20
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_LEFT = 0x30
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_UNKNOWN = 0xff
}

Macros#

#define
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_CLUSTER_SIZE 20
#define
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_DEVICE_TABLE_SIZE 250
#define
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_NULL_NODE_ID 0xffff
#define
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_NULL_INDEX 0xffff
#define
DEVICE_ID_ON_OFF_SWITCH 0x0000
#define
DEVICE_ID_LEVEL_CONTROL_SWITCH 0x0001
#define
DEVICE_ID_ON_OFF_OUTPUT 0x0002
#define
DEVICE_ID_LEVEL_CONTROL_OUTPUT 0x0003
#define
DEVICE_ID_SCENE_SELECTOR 0x0004
#define
DEVICE_ID_CONFIG_TOOL 0x0005
#define
DEVICE_ID_REMOTE_CONTROL 0x0006
#define
DEVICE_ID_COMBINED_INTERFACE 0x0007
#define
DEVICE_ID_RANGE_EXTENDER 0x0008
#define
DEVICE_ID_MAINS_POWER_OUTLET 0x0009
#define
DEVICE_ID_DOOR_LOCK 0x000a
#define
DEVICE_ID_DOOR_LOCK_CONTROLLER 0x000b
#define
DEVICE_ID_SIMPLE_SENSOR 0x000c
#define
DEVICE_ID_CONSUMPTION_AWARENESS_DEVICE 0x000d
#define
DEVICE_ID_HOME_GATEWAY 0x0050
#define
DEVICE_ID_SMART_PLUG 0x0051
#define
DEVICE_ID_WHITE_GOODS 0x0052
#define
DEVICE_ID_METER_INTERFACE 0x0053
#define
DEVICE_ID_ON_OFF_LIGHT 0x0100
#define
DEVICE_ID_DIMMABLE_LIGHT 0x0101
#define
DEVICE_ID_COLOR_DIMMABLE_LIGHT 0x0102
#define
DEVICE_ID_ON_OFF_LIGHT_SWITCH 0x0103
#define
DEVICE_ID_DIMMER_SWITCH 0x0104
#define
DEVICE_ID_COLOR_DIMMER_SWITCH 0x0105
#define
DEVICE_ID_LIGHT_SENSOR 0x0106
#define
DEVICE_ID_OCCUPANCY_SENSOR 0x0107
#define
DEVICE_ID_SHADE 0x0200
#define
DEVICE_ID_SHADE_CONTROLLER 0x0201
#define
DEVICE_ID_WINDOW_COVERING_DEVICE 0x0202
#define
DEVICE_ID_WINDOW_COVERING_CONTROLLER 0x0203
#define
DEVICE_ID_HEATING_COOLING_UNIT 0x0300
#define
DEVICE_ID_THERMOSTAT 0x0301
#define
DEVICE_ID_TEMPERATURE_SENSOR 0x0302
#define
DEVICE_ID_PUMP 0x0303
#define
DEVICE_ID_PUMP_CONTROLLER 0x0304
#define
DEVICE_ID_PRESSURE_SENSOR 0x0305
#define
DEVICE_ID_FLOW_SENSOR 0x0306
#define
DEVICE_ID_MINI_SPLIT_AC 0x0307
#define
DEVICE_ID_IAS_CIE 0x0400
#define
DEVICE_ID_IAS_ANCILLARY_CONTROL 0x0401
#define
DEVICE_ID_IAS_ZONE 0x0402
#define
DEVICE_ID_IAS_WARNING 0x0403

API Documentation#

sl_zigbee_af_device_table_cli_index_send#

void sl_zigbee_af_device_table_cli_index_send (uint16_t index)

Send a message using the device table.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the CLI command.

Sends the current framework ZCL command to the device specified by an index.


sl_zigbee_af_device_table_send#

void sl_zigbee_af_device_table_send (sl_802154_long_addr_t eui64, uint8_t endpoint)

Send a message using the device table.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

EUI64 to which to send the CLI command.

uint8_tN/Aendpoint

Endpoint of the device to which to send the CLI command.

Sends the current framework ZCL command using a device specified by the EUI64 and endpoint.


sl_zigbee_af_device_table_cli_index_send_with_endpoint#

void sl_zigbee_af_device_table_cli_index_send_with_endpoint (uint16_t index, uint8_t endpoint)

Send a CLI command based on an index and an endpoint.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends the current framework ZCL command using a device indexed in the device table.


sl_zigbee_af_device_table_command_index_send#

void sl_zigbee_af_device_table_command_index_send (uint16_t index)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

index of the device to which to send the command.

Sends an internally-generated command, such as generated by the sl_zigbee_af_fill_command_on_off_cluster_on(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


sl_zigbee_af_device_table_command_send_with_endpoint#

void sl_zigbee_af_device_table_command_send_with_endpoint (sl_802154_long_addr_t eui64, uint8_t endpoint)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

EUI64 of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends an internally-generated command, such as generated by the sl_zigbee_af_fill_command_on_off_cluster_on(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


sl_zigbee_af_device_table_command_index_send_with_endpoint#

void sl_zigbee_af_device_table_command_index_send_with_endpoint (uint16_t index, uint8_t endpoint)

Send an internally-generated command.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to which to send the command.

uint8_tN/Aendpoint

The endpoint of the device to which to send the command.

Sends an internally-generated command, such as generated by the sl_zigbee_af_fill_command_on_off_cluster_on(); command. Note: this is different from the above send command, which works with the CLI-generated outgoing commands.


sl_zigbee_af_device_table_get_eui64_from_node_id#

bool sl_zigbee_af_device_table_get_eui64_from_node_id (sl_802154_short_addr_t sl_zigbee_node_id, sl_802154_long_addr_t eui64)

Compute the EUI64 from the node ID in the device table.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/Asl_zigbee_node_id

The node ID of the device.

sl_802154_long_addr_tN/Aeui64

The location of the EUI64 variable.

This function looks up the device-table entry using the node ID and return the EUI64.

Returns

  • bool True if an EUI can be found, false if not.


sl_zigbee_af_device_table_get_node_id_from_index#

uint16_t sl_zigbee_af_device_table_get_node_id_from_index (uint16_t index)

Compute the node ID from the device table index.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device.

Looks up the device table entry based on the index and returns the node ID.

Returns

  • The node ID of the device.


sl_zigbee_af_device_table_get_endpoint_from_node_id_and_endpoint#

uint16_t sl_zigbee_af_device_table_get_endpoint_from_node_id_and_endpoint (sl_802154_short_addr_t sl_zigbee_node_id, uint8_t endpoint)

Find the endpoint index from node ID and endpoint number.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/Asl_zigbee_node_id

The node ID of the device.

uint8_tN/Aendpoint

The desired endpoint.

Computes the index into the endpoint table based on the node ID and the endpoint number.

Returns

  • The index of the device.


sl_zigbee_af_device_table_get_index_from_node_id#

uint16_t sl_zigbee_af_device_table_get_index_from_node_id (sl_802154_short_addr_t sl_zigbee_node_id)

Find the index based on the node ID.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/Asl_zigbee_node_id

The node ID of the current device.

Computes the device-table index based on the node ID.

Returns

  • The index in the device-table.


sl_zigbee_af_device_table_get_first_index_from_eui64#

uint16_t sl_zigbee_af_device_table_get_first_index_from_eui64 (sl_802154_long_addr_t eui64)

Find the index based on the EUI64.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

EUI64 of the desired node ID.

Computes the first device table index from the EUI64.

Returns

  • The first index that matches the EUI64.


sl_zigbee_af_device_table_get_index_from_eui64_and_endpoint#

uint16_t sl_zigbee_af_device_table_get_index_from_eui64_and_endpoint (sl_802154_long_addr_t eui64, uint8_t endpoint)

Find the index based on the EUI64 and endpoint.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

EUI64 of the desired index.

uint8_tN/Aendpoint

The endpoint for the desired index.

Computes the node ID based on the device table entry that matches the EUI64.

Returns

  • Index that matches the EUI64


sl_zigbee_af_device_table_get_node_id_from_eui64#

uint16_t sl_zigbee_af_device_table_get_node_id_from_eui64 (sl_802154_long_addr_t eui64)

Find the node ID based on the EUI64.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

EUI64 of the desired node ID.

Computes the node ID based on the device table entry that matches the EUI64.

Returns

  • The node ID that matches the EUI64.


sl_zigbee_af_device_table_message_sent_status#

void sl_zigbee_af_device_table_message_sent_status (sl_802154_short_addr_t nodeId, sl_status_t status, uint16_t profileId, uint16_t clusterId)

Change the device status based on the last sent message.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnodeId

The node ID in the last outgoing message.

sl_status_tN/Astatus

sl_status_t of the last outgoing message.

uint16_tN/AprofileId

The profile ID of the last outgoing message.

uint16_tN/AclusterId

The cluster ID of the last outgoing message.

If the last sent message was a success, change the device state to "joined". However, if the last message sent was not a success, change the device state to unresponsive.


sl_zigbee_af_device_table_send_leave#

void sl_zigbee_af_device_table_send_leave (uint16_t index)

Send a leave message to a device based on the index.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device to whom to send the leave message.

Sends a leave message to the device indicated by the index.


sl_zigbee_af_device_table_message_received#

void sl_zigbee_af_device_table_message_received (sl_802154_short_addr_t nodeId)

Inform the device table that a message was received.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnodeId

The node ID from which the last incoming message came.

The device table keeps track of whether a device has become unresponsive. Hearing from a known device causes the device table to transition the device state from "unresponsive" to "joined". Hearing from an unknown device causes the device table to discover the device, potentially fixing routing issues (i.e., if the node ID has changed).


sl_zigbee_af_device_table_initiate_route_repair#

void sl_zigbee_af_device_table_initiate_route_repair (sl_802154_short_addr_t nodeId)

Kick off device table route repair.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnodeId

The node ID of the newly unresponsive node.

A message was sent to the device and failed. Therefore, the route repair will be attempted and the node marked as unresponsive. Currently, route repair simply sends a broadcast message looking for the node ID based on the EUI64. It may be replaced with something more sophisticated in the future.


sl_zigbee_af_device_table_pointer#

sl_zigbee_af_plugin_device_table_entry_t * sl_zigbee_af_device_table_pointer (void )

Return a pointer to the device table structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns a pointer to the device table structure.

Returns

  • A pointer to the device table structure.


sl_zigbee_af_device_table_find_device_table_entry#

sl_zigbee_af_plugin_device_table_entry_t * sl_zigbee_af_device_table_find_device_table_entry (uint16_t index)

Return a pointer to the device table entry.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device table entry in which we are interested.

Returns a pointer to the device table entry based on the device table index.

Returns

  • A pointer to the device table entry.


sl_zigbee_af_device_table_new_device_join_handler#

void sl_zigbee_af_device_table_new_device_join_handler (sl_802154_short_addr_t newNodeId, sl_802154_long_addr_t newNodeEui64)

Inform the device table that a new device joined.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnewNodeId

The node ID of the newly joined device.

sl_802154_long_addr_tN/AnewNodeEui64

The EUI64 of the newly joined device.

Call this function in the device table when a device joins, rejoins, or sends an end-device announce. If the device is new, it will generate a new device table entry and kick off the discovery process. If the device is not new, the device-table will make sure the node ID matches the EUI64 and make an update if necessary. It will also check to verify the discovery process has completed and attempt to complete it.


sl_zigbee_af_device_table_time_since_last_message#

uint32_t sl_zigbee_af_device_table_time_since_last_message (uint16_t index)

Calculate time since the device heard the last message.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Aindex

The index of the device.

Computes the amount of time, in seconds, since receiving a message from the device.

Returns

  • The time since the last message (in seconds).


sl_zigbee_af_device_table_match_eui64#

bool sl_zigbee_af_device_table_match_eui64 (sl_802154_long_addr_t a, sl_802154_long_addr_t b)

Return true if the two EUI64 parameters match.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aa

The first EUI64 to compare.

sl_802154_long_addr_tN/Ab

The second EUI64 to compare.

Determines whether two EUI64 values are the same. The function will print a feedback message to indicate if both EUI64 values are NULL. The function will also print out a feedback message to indicate if the EUI64 values match but in reverse order.


sl_zigbee_af_device_table_clear#

void sl_zigbee_af_device_table_clear (void )

Clear the device table.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Clears the device table and the backup file of the device table is also cleared if it is a host.


sl_zigbee_af_device_table_index_removed_cb#

void sl_zigbee_af_device_table_index_removed_cb (uint16_t currentIndex)

Called when a device has been removed from the device table.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/AcurrentIndex

Index of the removed device.

Called when the device has been removed from the table.


sl_zigbee_af_device_table_initialized#

void sl_zigbee_af_device_table_initialized (void )

Called when the device table has been initialized.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Called when the device table has been initialized


Enumeration Documentation#

sl_zigbee_af_plugin_device_table_device_state_t#

sl_zigbee_af_plugin_device_table_device_state_t
Enumerator
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_NULL
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_JOINED
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_UNRESPONSIVE
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_LEAVE_SENT
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_LEFT
SL_ZIGBEE_AF_PLUGIN_DEVICE_TABLE_STATE_UNKNOWN

Typedef Documentation#

sl_zigbee_af_plugin_device_table_device_state_t#

typedef uint8_t sl_zigbee_af_plugin_device_table_device_state_t