Diagnostic Server#
API and Callbacks for the Diagnostic Cluster Server Component.
This component handles the retrieval of diagnostic information from the stack through the diagnostic cluster. Implement the component as follows:
1. Mark all diagnostic attributes you wish to track as external.
2. Add a call to sl_zigbee_af_read_diagnostic_attribute(attributeMetadata, buffer); from sl_zigbee_af_external_attribute_read_cb().
API#
bool
sl_zigbee_af_read_diagnostic_attribute(sl_zigbee_af_attribute_metadata_t *attributeMetadata, uint8_t *buffer)
Read diagnostic attributes.
API Documentation#
sl_zigbee_af_read_diagnostic_attribute#
bool sl_zigbee_af_read_diagnostic_attribute (sl_zigbee_af_attribute_metadata_t * attributeMetadata, uint8_t * buffer)
Read diagnostic attributes.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_zigbee_af_attribute_metadata_t * | N/A | attributeMetadata | Ver.: always |
uint8_t * | N/A | buffer | Ver.: always |
Returns
bool true is success