Zigbee Version 9.0 Revision 2 - Release Notes (May 4, 2026)#

Silicon Labs is the vendor of choice for OEMs developing Zigbee networking into their products. The Silicon Labs Zigbee platform is the most integrated, complete, and feature-rich Zigbee solution available.

Silicon Labs EmberZNet SDK contains Silicon Labs’ implementation of the Zigbee stack specification.

Click here for earlier releases.

Release Summary#

Release Item Version Release Date Release Notes Key Features API Changes Bug Fixes Chip Enablement

SDK

9.0 Revision 2

May 4, 2026

Release Notes

Refer to the Key Features section. Refer to the API Changes section. Refer to the Bug Fixes section. Refer to the Chip Enablement section.

802.15.4 Mesh + BLE Multiprotocol

9.0 Revision 2

May 4, 2026

Release Notes

Per-protocol TX power control in CMP applications. sl_802154_radio_set_scheduler_priorities() removed. Targeted quality improvements and bug fixes. None

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

This release contains the following:

  • Zigbee Stack

  • Zigbee Application Framework

  • Zigbee Sample Applications

For more information about Zigbee and the EmberZNet SDK see Zigbee Fundamentals.

If you are a first-time user, see Zigbee EmberZNet Quick-Start Guide for SDK 7.0 and Higher, for instructions on configuring your development environment, building and flashing a sample application, and documentation references pointing to next steps.

Compatible Software#

Compatibility and Use Notices: For information about security updates and notices, see the Security chapter of the Platform Release Notes installed with this SDK or on the TECH DOCS tab on https://www.silabs.com/developers/zigbee-emberznet. Silicon Labs also strongly recommends that you subscribe to Security Advisories for up-to-date information.

For instructions, or if you are new to the Zigbee EmberZNet SDK, see Using This Release.

Software Compatible Version or Variant

IAR Embedded Workbench for ARM (IAR-EWARM)

Using wine to build with the IarBuild.exe command line utility or IAR Embedded Workbench GUI on macOS or Linux could result in incorrect files being used due to collisions in wine’s hashing algorithm for generating short file names.

Customers on macOS or Linux are advised not to build with IAR outside of Simplicity Studio. Customers who do should carefully verify that the correct files are being used.

Note: Users are reminded that applications intended for Series 3 parts are not supported with the IAR toolchain in this release.

Version 9.40.1
GCC (The GNU Compiler Collection) Version 12.2.1
EZSP Protocol Version 0x12

Installation and Use#

To run your first demo, see our Getting Started Guide.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation.

Additional Information#

Zigbee Certification

The EmberZNet 9.0 release is qualified as a Zigbee Compliant Platform for SoC, NCP and RCP architectures. For ZCP certification ID tied to this release, please check the CSA website here: https://csa-iot.org/csa-iot_products/.

Note that the ZCP certification is filed post-release and takes a few weeks before getting reflected on the CSA website. For any further queries, please contact Silicon Laboratories support at http://www.silabs.com/support.

Help and Feedback#

Feature Matrix#

Supported Features | Unsupported Features

Supported Features#

Feature Name Description Quality Related API Names Supported Software Variants, Hardware, Modes, Host Interfaces Related Example Names
Zigbee 4.0 compliance with BDB 3.1 and R23 support This release is Zigbee 4.0 certification-ready, with BDB 3.1 and R23 features incorporated. Production SoC
Host-NCP
Zigbee - Z4Light
Zigbee - Z4Switch
Dynamic switching of Zigbee node type between router and sleepy end device This feature allows an image to dynamically switch between a router and a sleepy end device at runtime. This is not to be confused with the multi-network feature, where an image can be configured with two device types operating on different networks (for that, see AN724). Production sl_zigbee_af_switch_role_router
sl_zigbee_af_switch_role_sleepy_end_device
SoC
All
Inter-PAN messages filtering update Updated filtering of inter-PAN message to support multiple filters matching regardless of whether ZLL or custom filters match. The matched filter value will be passed up to the application using sli_802154_stack_filter_match_message_handler(). Production sl_zigbee_af_mac_filter_match_message_cb
sl_zigbee_ezsp_mac_filter_match_message_handler
sl_802154_filter_match_message_handler
SoC
Host-NCP
All

Unsupported Features#

Feature Name Description Quality Related API Names Supported Software Variants, Hardware, Modes, Host Interfaces Related Example Names
IAR toolchain for Series 3 Users are reminded that applications intended for Series 3 parts are not supported with the IAR toolchain in this release. Production


SoC
NCP
CPC
Series 3
Zigbee NCP SPI Applications on Series 3 Applications utilizing direct SPI access (that is, without the use of CPC) are currently not working for Series 3 hardware. This includes the "Zigbee - NCP ncp-spi" and "Zigbee - NCP MpNcpSpi" applications, as well as any application that brings in the "NCP SPI" component. Generations of such applications will fail, indicating unmet dependencies or incompatible dependencies. Production NA
NCP SPI
Series 3

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.