End Device Support#
API and Callbacks for the End Device Support Component.
Silicon Labs implementation of polling for end devices. Note that the Poll Control Server component sets the long and short poll intervals at startup. If both components are enabled, the long and short poll intervals set here will not be used.
Modules#
Handlers#
void
sl_zigbee_af_end_device_support_move_network_event_handler(sl_zigbee_af_event_t *event)
End Device Support Move Network Event Handler.
Handlers Documentation#
sl_zigbee_af_end_device_support_move_network_event_handler#
void sl_zigbee_af_end_device_support_move_network_event_handler (sl_zigbee_af_event_t * event)
End Device Support Move Network Event Handler.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_event_t * | [in] | event | a type sl_zigbee_af_event_t |
This API handles the stack logic when there is a Move Network Event Scheduled. This handler will attempt to call: sl_zigbee_find_and_rejoin_network to move networks. This handler will either be completed upon a successful move or upon failure will reschedule a new move network event until a maximum number of retry events.