WWAH App Event Retry Manager#

API and Callbacks for the WWAH App Event Retry Manager Component.

Silicon Labs proprietary Works With All Hubs (WWAH) app event retry manager.

Modules#

WWAH App Event Retry manager

API#

void

Write attribute-enabled callback.

void

Write attribute queue size callback.

void

WWAH app event retry manager set backoff parameters to default.

API Documentation#

sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled#

void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled (uint8_t enabled)

Write attribute-enabled callback.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aenabled

Ver.: always

This callback is called when the enabled backoff parameter is changed.


sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size#

void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size (uint8_t queueSize)

Write attribute queue size callback.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/AqueueSize

Ver.: always

This callback is called when the app event retry queue size is being reported.


sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default#

void sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default (void )

WWAH app event retry manager set backoff parameters to default.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This callback is called when the app event retry manager is about to set the backoff parameters of the critical message queue provider plugin back to their default.