Complete events with a control and a handler procedure.

An application typically creates an array of events along with their handlers. The main loop passes the array to ::sl_zigbee_run_events() to call the handlers of any events whose time has arrived.

Public Attribute Documentation#

control#

sl_zigbee_event_control_t* sl_zigbee_event_data_t::control

The control structure for the event.


Definition at line 1816 of file stack/include/sl_zigbee_types.h

handler#

void(* sl_zigbee_event_data_t::handler) (void)

The procedure to call when the event fires.


Definition at line 1818 of file stack/include/sl_zigbee_types.h