This data structure contains the transient key data that is used during Zigbee 3.0 joining.

Public Attributes#

sl_802154_long_addr_t
uint32_t
union sl_zigbee_transient_key_data_t::@1

Public Attribute Documentation#

eui64#

sl_802154_long_addr_t sl_zigbee_transient_key_data_t::eui64

Definition at line 2342 of file stack/include/sl_zigbee_types.h

incomingFrameCounter#

uint32_t sl_zigbee_transient_key_data_t::incomingFrameCounter

Definition at line 2343 of file stack/include/sl_zigbee_types.h

bitmask#

sl_zigbee_key_struct_bitmask_t sl_zigbee_transient_key_data_t::bitmask

Definition at line 2344 of file stack/include/sl_zigbee_types.h

remainingTimeSeconds#

uint16_t sl_zigbee_transient_key_data_t::remainingTimeSeconds

Definition at line 2345 of file stack/include/sl_zigbee_types.h

networkIndex#

uint8_t sl_zigbee_transient_key_data_t::networkIndex

Definition at line 2346 of file stack/include/sl_zigbee_types.h

keyData#

sl_zigbee_key_data_t sl_zigbee_transient_key_data_t::keyData

Definition at line 2348 of file stack/include/sl_zigbee_types.h

psa_id#

uint32_t sl_zigbee_transient_key_data_t::psa_id

Definition at line 2349 of file stack/include/sl_zigbee_types.h

@2#

union sl_zigbee_transient_key_data_t::@1 sl_zigbee_transient_key_data_t::@2

Definition at line 2350 of file stack/include/sl_zigbee_types.h