Modules#
sl_bt_evt_gatt_procedure_completed_s
sl_bt_evt_gatt_procedure_completed#
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
All GATT commands excluding sl_bt_gatt_write_characteristic_value_without_response and sl_bt_gatt_send_characteristic_confirmation will trigger this event. As a result, the application must wait for this event before issuing another GATT command (excluding the two aforementioned exceptions).
Note: After a failed GATT procedure with SL_STATUS_TIMEOUT error, further GATT transactions over this connection are not allowed by the stack.
Typedefs#
Macros#
#define
sl_bt_evt_gatt_procedure_completed_id 0x060900a0
Identifier of the procedure_completed event.