Advertiser PAST#
Advertiser PAST.
Transfer the synchronization information of a local active periodic advertising set to a remote device using Periodic Advertising Synchronization Transfer (PAST) over a connection.
Functions#
sl_status_t
sl_bt_advertiser_past_transfer(uint8_t connection, uint16_t service_data, uint8_t advertising_set)
Macros#
#define
sl_bt_cmd_advertiser_past_transfer_id 0x00520020
#define
sl_bt_rsp_advertiser_past_transfer_id 0x00520020
Function Documentation#
sl_bt_advertiser_past_transfer#
sl_status_t sl_bt_advertiser_past_transfer (uint8_t connection, uint16_t service_data, uint8_t advertising_set)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle of the connection used to transmit the sync transfer | 
| uint16_t | [in] | service_data | A value provided by the application for use by the peer device. | 
| uint8_t | [in] | advertising_set | Handle of the periodic advertising set to transfer | 
Transfer the synchronization information of an advertising set that is actively performing periodic advertising.
Returns
- SL_STATUS_OK if successful. Error code otherwise.