Periodic Advertising with responses Synchronization#
Periodic Advertising with responses Synchronization.
Provides events and control for synchronized Periodic Advertising with Responses (PAwR) trains. Synchronization is achieved by scanning (see Periodic Advertising Sync Scanner) or by receiving Periodic Advertising Synchronization Transfer (see PAST Receiver).
Modules#
sl_bt_evt_pawr_sync_transfer_received
sl_bt_evt_pawr_sync_subevent_report
Functions#
Macros#
Function Documentation#
sl_bt_pawr_sync_set_sync_subevents#
sl_status_t sl_bt_pawr_sync_set_sync_subevents (uint16_t sync, size_t subevents_len, const uint8_t *subevents)
[in] | sync | PAwR synchronization handle |
[in] | subevents_len | Length of data in |
[in] | subevents | Array of subevent indexes to synchronize to |
Specify the subevents that this device will synchronize to on the specified PAwR train.
Returns
SL_STATUS_OK if successful. Error code otherwise.
5947
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_pawr_sync_set_response_data#
sl_status_t sl_bt_pawr_sync_set_response_data (uint16_t sync, uint16_t request_event, uint8_t request_subevent, uint8_t response_subevent, uint8_t response_slot, size_t response_data_len, const uint8_t *response_data)
[in] | sync | PAwR synchronization handle |
[in] | request_event | The periodic advertising event counter (paEventCounter) of the request. Set this parameter to the value of the |
[in] | request_subevent | The subevent of the request. Set this parameter to the value of the |
[in] | response_subevent | The subevent in which the response is to be sent |
[in] | response_slot | The response slot in which the response is to be sent |
[in] | response_data_len | Length of data in |
[in] | response_data | Data to be sent in the specified response slot. Maximum of 248 bytes of data can be set with this command. |
Set the data to be sent in the specified response slot of a subevent of an active PAwR train.
Use this command when the application receives the sl_bt_evt_pawr_sync_subevent_report event and the application needs to send a response. The application needs to set the response data within the timing requirements implied by the parameters of the PAwR train that the device is synchronized to. If the response data is set too late, this command will fail with result SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT.
Returns
SL_STATUS_OK if successful. Error code otherwise.
5982
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_cmd_pawr_sync_set_sync_subevents_id#
#define sl_bt_cmd_pawr_sync_set_sync_subevents_idValue:
0x02540020
5670
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_pawr_sync_set_response_data_id#
#define sl_bt_cmd_pawr_sync_set_response_data_idValue:
0x03540020
5671
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_pawr_sync_set_sync_subevents_id#
#define sl_bt_rsp_pawr_sync_set_sync_subevents_idValue:
0x02540020
5672
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_pawr_sync_set_response_data_id#
#define sl_bt_rsp_pawr_sync_set_response_data_idValue:
0x03540020
5673
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h