BT Common Types#
BT common types.
Modules#
Macros#
#define
SL_BT_INVALID_CONNECTION_HANDLE ((uint8_t) 0xFF)
Value used to indicate an invalid connection handle.
#define
SL_BT_INVALID_BONDING_HANDLE ((uint8_t) 0xFF)
Value used to indicate an invalid bonding handle.
#define
SL_BT_INVALID_ADVERTISING_SET_HANDLE ((uint8_t) 0xFF)
Value used to indicate an invalid advertising set handle.
#define
SL_BT_INVALID_SYNC_HANDLE ((uint16_t) 0xFFFF)
Value used to indicate an invalid sync handle.
Typedef Documentation#
sl_bt_msg_t#
typedef struct sl_bt_msg sl_bt_msg_t
Type definition for the data structure of BT API messages.
Macro Definition Documentation#
SL_BT_INVALID_CONNECTION_HANDLE#
#define SL_BT_INVALID_CONNECTION_HANDLEValue:
((uint8_t) 0xFF)
Value used to indicate an invalid connection handle.
SL_BT_INVALID_BONDING_HANDLE#
#define SL_BT_INVALID_BONDING_HANDLEValue:
((uint8_t) 0xFF)
Value used to indicate an invalid bonding handle.
SL_BT_INVALID_ADVERTISING_SET_HANDLE#
#define SL_BT_INVALID_ADVERTISING_SET_HANDLEValue:
((uint8_t) 0xFF)
Value used to indicate an invalid advertising set handle.
SL_BT_INVALID_SYNC_HANDLE#
#define SL_BT_INVALID_SYNC_HANDLEValue:
((uint16_t) 0xFFFF)
Value used to indicate an invalid sync handle.