CTE Transmitter#
CTE Transmitter.
Commands and events in this class manage Constant Tone Extension (CTE) transmission.
CTE feature is only supported by specific devices. Commands from this class will return SL_STATUS_NOT_SUPPORTED on devices that do not support CTE.
Functions#
Macros#
Function Documentation#
sl_bt_cte_transmitter_set_dtm_parameters#
sl_status_t sl_bt_cte_transmitter_set_dtm_parameters (uint8_t cte_length, uint8_t cte_type, size_t switching_pattern_len, const uint8_t * switching_pattern)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | cte_length | The length of the Constant Tone Extension in 8 us units 
 Default: 0 (no CTE) | 
| uint8_t | [in] | cte_type | CTE type 
 Default: 0 | 
| size_t | [in] | switching_pattern_len | Length of data in  | 
| const uint8_t * | [in] | switching_pattern | Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over. This can be an empty array if CTE is unused. | 
Set the CTE-related parameters of the LE transmitter test.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_clear_dtm_parameters#
sl_status_t sl_bt_cte_transmitter_clear_dtm_parameters ()
Clear CTE-related parameters that were previously set for LE transmitter test. Default values will be restored for these parameters.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_enable_connection_cte#
sl_status_t sl_bt_cte_transmitter_enable_connection_cte (uint8_t connection, uint8_t cte_types, size_t switching_pattern_len, const uint8_t * switching_pattern)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle | 
| uint8_t | [in] | cte_types | CTE types. Bitmask of the following: 
 | 
| size_t | [in] | switching_pattern_len | Length of data in  | 
| const uint8_t * | [in] | switching_pattern | Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over. | 
Enable different types of CTE responses on a connection. CTE response will be sent once requested by the peer device using the CTE Request procedure.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_disable_connection_cte#
sl_status_t sl_bt_cte_transmitter_disable_connection_cte (uint8_t connection)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle | 
Disable CTE responses on a connection.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_enable_connectionless_cte#
sl_status_t sl_bt_cte_transmitter_enable_connectionless_cte (uint8_t handle, uint8_t cte_length, uint8_t cte_type, uint8_t cte_count, size_t switching_pattern_len, const uint8_t * switching_pattern)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | handle | Periodic advertising handle | 
| uint8_t | [in] | cte_length | CTE length in 8 us units. 
 | 
| uint8_t | [in] | cte_type | CTE type 
 | 
| uint8_t | [in] | cte_count | The number of CTEs to be transmitted in each periodic advertising interval | 
| size_t | [in] | switching_pattern_len | Length of data in  | 
| const uint8_t * | [in] | switching_pattern | Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over. | 
Start a connectionless CTE transmit. CTEs will be transmitted in periodic advertisement packets. As a result, a periodic advertising has to be started prior to this command.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_disable_connectionless_cte#
sl_status_t sl_bt_cte_transmitter_disable_connectionless_cte (uint8_t handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | handle | Periodic advertising handle | 
Stop the connectionless CTE transmit.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_enable_silabs_cte#
sl_status_t sl_bt_cte_transmitter_enable_silabs_cte (uint8_t handle, uint8_t cte_length, uint8_t cte_type, uint8_t cte_count, size_t switching_pattern_len, const uint8_t * switching_pattern)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | handle | Advertising handle | 
| uint8_t | [in] | cte_length | CTE length in 8 us units. 
 | 
| uint8_t | [in] | cte_type | CTE type 
 | 
| uint8_t | [in] | cte_count | The number of CTEs to be transmitted in each extended advertising interval. Currently, only cte_count = 1 is supported. | 
| size_t | [in] | switching_pattern_len | Length of data in  | 
| const uint8_t * | [in] | switching_pattern | Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over. | 
Enable Silicon Labs CTE transmit. CTEs will be transmitted in extended advertisement packets. As a result, extended advertising has to be started prior this command.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_cte_transmitter_disable_silabs_cte#
sl_status_t sl_bt_cte_transmitter_disable_silabs_cte (uint8_t handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | handle | Advertising handle | 
Disable Silicon Labs CTE transmit.
Returns
- SL_STATUS_OK if successful. Error code otherwise.