Data structure of the error event.
Public Attribute Documentation#
reason#
uint16_t sl_bt_evt_system_error_s::reason
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
829
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
data#
uint8array sl_bt_evt_system_error_s::data
Data related to the error; this field can be empty.
Definition at line
830
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h