sl_bt_evt_dfu_boot#

This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).

Modules#

sl_bt_evt_dfu_boot_s

Macros#

#define

Identifier of the boot event.

Typedef Documentation#

sl_bt_evt_dfu_boot_t#

typedef struct sl_bt_evt_dfu_boot_s sl_bt_evt_dfu_boot_t

Definition at line 154 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_dfu_boot_id#

#define sl_bt_evt_dfu_boot_id
Value:
0x000000a0

Identifier of the boot event.


Definition at line 144 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h