Data structure of the mtu_exchanged event.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_mtu_exchanged_s::connection

Connection handle


Definition at line 8008 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

mtu#

uint16_t sl_bt_evt_gatt_mtu_exchanged_s::mtu

Exchanged ATT_MTU


Definition at line 8009 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h