Data structure of the closed event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

reason#

uint16_t sl_bt_evt_sync_closed_s::reason

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 4868 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sync#

uint16_t sl_bt_evt_sync_closed_s::sync

Periodic advertising synchronization handle


Definition at line 4869 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h