sl_bt_evt_system_external_signal#
Indicates that the external signals have been received.
External signals are generated from the native application.
Modules#
sl_bt_evt_system_external_signal_s
Typedefs#
Macros#
#define
sl_bt_evt_system_external_signal_id 0x030100a0
Identifier of the external_signal event.
Typedef Documentation#
sl_bt_evt_system_external_signal_t#
typedef struct sl_bt_evt_system_external_signal_s sl_bt_evt_system_external_signal_t
Definition at line
943
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_system_external_signal_id#
#define sl_bt_evt_system_external_signal_idValue:
0x030100a0
Identifier of the external_signal event.
Definition at line
932
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h