Data structure of the silabs_iq_report event.

Public Attributes#

uint16_t
uint8_t
uint8_t
int8_t
uint8_t

Public Attribute Documentation#

status#

uint16_t sl_bt_evt_cte_receiver_silabs_iq_report_s::status

Status of CTE IQ sampling


address#

bd_addr sl_bt_evt_cte_receiver_silabs_iq_report_s::address

Bluetooth address of the remote device


address_type#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::address_type

Enum sl_bt_gap_address_type_t.

Advertiser address type.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:

  • 0: Public address

  • 1: Random address

  • 255: No address provided (anonymous advertising)

If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_anonymous_address (0xff): No address provided (anonymous advertising)

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


phy#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::phy

The PHY on which the packet is received.

  • 1: 1M PHY

  • 2: 2M PHY


channel#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::channel

The channel on which the CTE packet was received


rssi#

int8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::rssi

RSSI in the received CTE packet. Unit: dBm


rssi_antenna_id#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::rssi_antenna_id

The ID of the antenna on which RSSI was measured


cte_type#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::cte_type

The CTE type

  • 0: AoA CTE response

  • 1: AoD CTE response with 1us slots

  • 2: AoD CTE response with 2us slots


slot_durations#

uint8_t sl_bt_evt_cte_receiver_silabs_iq_report_s::slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each


packet_counter#

uint16_t sl_bt_evt_cte_receiver_silabs_iq_report_s::packet_counter

The event counter of the periodic advertising train or the connection


samples#

uint8array sl_bt_evt_cte_receiver_silabs_iq_report_s::samples

IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...)