sl_bt_evt_gatt_descriptor_value#
Indicates that the value of a descriptor in the remote GATT server was received.
This event is generated by the sl_bt_gatt_read_descriptor_value command.
Modules#
sl_bt_evt_gatt_descriptor_value_s
Typedefs#
Macros#
#define
sl_bt_evt_gatt_descriptor_value_id 0x050900a0
Identifier of the descriptor_value event.
Typedef Documentation#
sl_bt_evt_gatt_descriptor_value_t#
typedef struct sl_bt_evt_gatt_descriptor_value_s sl_bt_evt_gatt_descriptor_value_t
Definition at line
7239
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_descriptor_value_id#
#define sl_bt_evt_gatt_descriptor_value_idValue:
0x050900a0
Identifier of the descriptor_value event.
Definition at line
7226
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h