You are viewing documentation for version:
sl_bt_evt_sm_passkey_request#
Indicates a request for the passkey prompt displayed on the remote device.
Use the command sl_bt_sm_enter_passkey to input the passkey value.
Modules#
sl_bt_evt_sm_passkey_request_s
Macros#
#define
Identifier of the passkey_request event.
Typedef Documentation#
sl_bt_evt_sm_passkey_request_t#
typedef struct sl_bt_evt_sm_passkey_request_s sl_bt_evt_sm_passkey_request_t
Definition at line 9885
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_sm_passkey_request_id#
#define sl_bt_evt_sm_passkey_request_id
Value:0x010f00a0
Identifier of the passkey_request event.
Definition at line 9875
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h