Data structure of the closed event.
Public Attribute Documentation#
reason#
uint16_t sl_bt_evt_sync_closed_s::reason
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
3923
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sync#
uint16_t sl_bt_evt_sync_closed_s::sync
Periodic advertising synchronization handle
Definition at line
3924
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h