You are viewing documentation for version:
sl_bt_evt_system_error#
Indicates that an error has occurred.
See error codes table for more information.
Modules#
sl_bt_evt_system_error_s
Macros#
#define
Identifier of the error event.
Typedef Documentation#
sl_bt_evt_system_error_t#
typedef struct sl_bt_evt_system_error_s sl_bt_evt_system_error_t
Definition at line 826
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_system_error_id#
#define sl_bt_evt_system_error_id
Value:0x060100a0
Identifier of the error event.
Definition at line 815
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h