Extended Advertising Configuration Flags#
This enum defines configuration flags for the extended advertising.
Macros#
#define
Macro Definition Documentation#
SL_BT_EXTENDED_ADVERTISER_ANONYMOUS_ADVERTISING#
#define SL_BT_EXTENDED_ADVERTISER_ANONYMOUS_ADVERTISINGValue:
0x1
Omit advertiser's address from all PDUs (anonymous advertising). The advertising cannot be connectable or scannable if this flag is set.
Definition at line
2664
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
SL_BT_EXTENDED_ADVERTISER_INCLUDE_TX_POWER#
#define SL_BT_EXTENDED_ADVERTISER_INCLUDE_TX_POWERValue:
0x2
Include the TX power in advertising packets.
Definition at line
2667
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h