Event Type Flags of Advertisement Reports#
Defines the event type flags of the advertisement packets the scanner reports. An advertisement packet could have multiple applicable flags.
Macro Definition Documentation#
SL_BT_SCANNER_EVENT_FLAG_CONNECTABLE#
#define SL_BT_SCANNER_EVENT_FLAG_CONNECTABLEValue:
0x1
A connectable advertising data packet
Definition at line
3324
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
SL_BT_SCANNER_EVENT_FLAG_SCANNABLE#
#define SL_BT_SCANNER_EVENT_FLAG_SCANNABLEValue:
0x2
A scannable advertising data packet
Definition at line
3327
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
SL_BT_SCANNER_EVENT_FLAG_DIRECTED#
#define SL_BT_SCANNER_EVENT_FLAG_DIRECTEDValue:
0x4
Directed advertising
Definition at line
3330
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
SL_BT_SCANNER_EVENT_FLAG_SCAN_RESPONSE#
#define SL_BT_SCANNER_EVENT_FLAG_SCAN_RESPONSEValue:
0x8
A scan response packet that can be received in active scan mode only
Definition at line
3333
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h