sl_bt_evt_connection_parameters#

Triggered whenever the connection parameters are changed and at any time a connection is established.

Modules#

sl_bt_evt_connection_parameters_s

Macros#

#define
sl_bt_evt_connection_parameters_id 0x020600a0

Identifier of the parameters event.

Typedef Documentation#

sl_bt_evt_connection_parameters_t#

typedef struct sl_bt_evt_connection_parameters_s sl_bt_evt_connection_parameters_t

Definition at line 5651 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h