Data structure of the procedure_completed event.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_procedure_completed_s::connection

Connection handle


Definition at line 7296 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

result#

uint16_t sl_bt_evt_gatt_procedure_completed_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 7297 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h