sl_bt_evt_gatt_server_characteristic_status#
Indicates either that a local Client Characteristic Configuration descriptor was changed by the remote GATT client, or that a confirmation from the remote GATT client was received upon a successful reception of the indication.
A confirmation by the remote GATT client should be received within 30 seconds after an indication was sent with the sl_bt_gatt_server_send_indication command, otherwise further GATT transactions over this connection are not allowed by the stack.
Modules#
sl_bt_evt_gatt_server_characteristic_status_s
Typedefs#
Macros#
#define
sl_bt_evt_gatt_server_characteristic_status_id 0x030a00a0
Identifier of the characteristic_status event.
Typedef Documentation#
sl_bt_evt_gatt_server_characteristic_status_t#
typedef struct sl_bt_evt_gatt_server_characteristic_status_s sl_bt_evt_gatt_server_characteristic_status_t
Definition at line
8825
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h