Data structure of BT API messages.

Public Attributes#

uint32_t
union sl_bt_msg::@0

Public Attribute Documentation#

header#

uint32_t sl_bt_msg::header

API protocol header consisting of event identifier and data length


Definition at line 14852 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

data#

union sl_bt_msg::@0 sl_bt_msg::data

Union of API event types


Definition at line 14936 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h