Data structure of the closed event.
Public Attribute Documentation#
reason#
uint16_t sl_bt_evt_connection_closed_s::reason
Reason of connection close.
Error code SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT indicates that the high duty cycle directed advertising timed out and no connection was established. Ignore the value of connection
in this case.
Definition at line
6425
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
connection#
uint8_t sl_bt_evt_connection_closed_s::connection
Handle of the closed connection
Definition at line
6432
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h