Bluetooth Mesh Light Control Setup Server Model#

Bluetooth Mesh Light Control Setup Server Model.

Bluetooth Mesh Light Control model Setup Server functionality.

This class provides the API that the LC Setup server uses to inform the application of its received events. The API is informational: application is not required to react to these events.

Modules#

sl_btmesh_evt_lc_setup_server_set_property

Functions#

sl_status_t
sl_btmesh_lc_setup_server_update_property(uint16_t elem_index, uint16_t property_id, size_t params_len, const uint8_t *params)

Function Documentation#

sl_btmesh_lc_setup_server_update_property#

sl_status_t sl_btmesh_lc_setup_server_update_property (uint16_t elem_index, uint16_t property_id, size_t params_len, const uint8_t * params)
Parameters
[in]elem_index

Client model element index

[in]property_id

Property ID for the LC Server. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.

[in]params_len

Length of data in params

[in]params

Byte array containing serialized fields of LC Property, excluding the property ID

Update the LC Server property. The application may choose to directly set model properties in the stack. This function will pass the property value to the LC Setup Server and on to the LC Server model.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14498 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_cmd_lc_setup_server_update_property_id#

#define sl_btmesh_cmd_lc_setup_server_update_property_id
Value:
0x004e0028

Definition at line 14451 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_lc_setup_server_update_property_id#

#define sl_btmesh_rsp_lc_setup_server_update_property_id
Value:
0x004e0028

Definition at line 14452 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h