Bluetooth Mesh Generic Client Model#
Bluetooth Mesh Generic Client Model.
Generic client model API provides a functionality to send and receive messages using Bluetooth SIG client models, including generic client models and lighting client models.
In the API, the client model that is used is identified by its element address and model ID, while the server model responding to client model requests is identified by its element address and model ID.
The API has functions for querying server model states, requesting server model state changes, and publishing messages. The application has to implement more complex functionality (state machines or other model-specific logic).
Data for state change requests and server responses is passed as serialized byte arrays through BGAPI. There are functions to convert byte arrays to and from model state structures in the Bluetooth mesh SDK.
The stack will handle Mesh transaction layer segmentation and reassembly automatically if the messages sent are long enough to require it.
Note on time resolution
Because of message formatting, transition time and remaining time resolution units depend on the requested or reported value. For example, until 6.2 seconds it is 100 ms; until 62 seconds it is 1 s; until 620 seconds it is 10 s; and until 620 minutes it is 10 minutes. The value cannot be longer than 620 minutes. Therefore, it is not possible to request a delay of exactly 7500 ms. The resolution unit is 1 s between 6.2 and 62 seconds, so the value would be rounded down to 7 s.
Delay resolution is 5 ms and values will be rounded down to the closest 5 ms. The value can't be longer than 1275 ms.
Modules#
Generic Client Get State Types
Generic Client Set Request Types
sl_btmesh_evt_generic_client_server_status
Functions#
Macros#
Function Documentation#
sl_btmesh_generic_client_get#
sl_status_t sl_btmesh_generic_client_get (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | model_id | Client model ID |
| uint16_t | [in] | appkey_index | The application key index to use |
| uint8_t | [in] | type | Model-specific state type, identifying the kind of state to retrieve. See Generic Client Get State Types list for details. |
Get the current state of a server model or models in the network. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.
The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_generic_client_set#
sl_status_t sl_btmesh_generic_client_set (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t * parameters)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | model_id | Client model ID |
| uint16_t | [in] | appkey_index | The application key index to use |
| uint8_t | [in] | tid | Transaction identifier. This applies to those messages the Mesh Model specification defines as transactional and can be left as zero for others. |
| uint32_t | [in] | transition_ms | Transition time (in milliseconds) for the state change. If both the transition time and the delay are zero, the transition is immediate. This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others. |
| uint16_t | [in] | delay_ms | Delay time (in milliseconds) before starting the state change. If both the transition time and the delay are zero, the transition is immediate. This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others. |
| uint16_t | [in] | flags | Message flags. Bitmask of the following:
|
| uint8_t | [in] | type | Model-specific request type. See set request types list for details. |
| size_t | [in] | parameters_len | Length of data in |
| const uint8_t * | [in] | parameters | Message-specific set request parameters serialized into a byte array |
Set the current state of a server model or models in the network. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.
The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events. Note that for responses to be generated the corresponding flag needs to be set.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_generic_client_publish#
sl_status_t sl_btmesh_generic_client_publish (uint16_t elem_index, uint16_t model_id, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t * parameters)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | model_id | Client model ID |
| uint8_t | [in] | tid | Transaction identifier |
| uint32_t | [in] | transition_ms | Transition time (in milliseconds) for the state change. If both the transition time and the delay are zero, the transition is immediate. This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others. |
| uint16_t | [in] | delay_ms | Delay time (in milliseconds) before starting the state change. If both the transition time and the delay are zero, the transition is immediate. This applies to messages the Mesh Model specification defines to have transition and delay times, and can be left as zero for others. |
| uint16_t | [in] | flags | Message flags. Bitmask of the following:
|
| uint8_t | [in] | type | Model-specific request type. See set request types list for details. |
| size_t | [in] | parameters_len | Length of data in |
| const uint8_t * | [in] | parameters | Message-specific set request parameters serialized into a byte array |
Publish a set request to the network using the publish address and publish application key of the model. The message will be received by the server models which subscribe to the publish address, and there's no need to explicitly specify a destination address or application key.
The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events. To generate responses, the corresponding flag needs to be set.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_generic_client_get_params#
sl_status_t sl_btmesh_generic_client_get_params (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type, size_t parameters_len, const uint8_t * parameters)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | model_id | Client model ID |
| uint16_t | [in] | appkey_index | The application key index to use. |
| uint8_t | [in] | type | Model-specific state type, identifying the kind of state to retrieve. See Generic Client Get State Types list for details. |
| size_t | [in] | parameters_len | Length of data in |
| const uint8_t * | [in] | parameters | Message-specific get request parameters serialized into a byte array |
Get the current state of a server model or models in the network, with additional parameters detailing the request. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.
The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events.
This call is used to query properties, for which the property ID is given as a parameter.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_generic_client_init#
sl_status_t sl_btmesh_generic_client_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic and lighting client models. This command initializes all generic and lighting client models on the device. Alternatively, only the necessary client models can be initialized using model-specific initialization commands. Using model-specific initialization can result in a smaller firmware image size for SoC projects.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_common#
sl_status_t sl_btmesh_generic_client_init_common (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize the generic client model common functionality. This command should be called only after all model-specific initialization calls for all generic and lighting client models on the device are done. An error will be returned if some of the generic and lighting client models were not initialized before calling this API. It does not need to be called if sl_btmesh_generic_client_init is used.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_on_off#
sl_status_t sl_btmesh_generic_client_init_on_off (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic on/off client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_level#
sl_status_t sl_btmesh_generic_client_init_level (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic level client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_default_transition_time#
sl_status_t sl_btmesh_generic_client_init_default_transition_time (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic default transition time client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_power_on_off#
sl_status_t sl_btmesh_generic_client_init_power_on_off (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic power on/off client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_power_level#
sl_status_t sl_btmesh_generic_client_init_power_level (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic power level client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_battery#
sl_status_t sl_btmesh_generic_client_init_battery (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic battery client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_location#
sl_status_t sl_btmesh_generic_client_init_location (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic location client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_property#
sl_status_t sl_btmesh_generic_client_init_property (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize generic property client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_lightness#
sl_status_t sl_btmesh_generic_client_init_lightness (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize light lightness client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_ctl#
sl_status_t sl_btmesh_generic_client_init_ctl (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize light CTL client models.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_generic_client_init_hsl#
sl_status_t sl_btmesh_generic_client_init_hsl (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize light HSL client models
Returns
SL_STATUS_OK if successful. Error code otherwise.
Macro Definition Documentation#
sl_btmesh_cmd_generic_client_publish_id#
#define sl_btmesh_cmd_generic_client_publish_idValue:
0x021e0028
sl_btmesh_cmd_generic_client_get_params_id#
#define sl_btmesh_cmd_generic_client_get_params_idValue:
0x031e0028
sl_btmesh_cmd_generic_client_init_common_id#
#define sl_btmesh_cmd_generic_client_init_common_idValue:
0x051e0028
sl_btmesh_cmd_generic_client_init_on_off_id#
#define sl_btmesh_cmd_generic_client_init_on_off_idValue:
0x061e0028
sl_btmesh_cmd_generic_client_init_level_id#
#define sl_btmesh_cmd_generic_client_init_level_idValue:
0x071e0028
sl_btmesh_cmd_generic_client_init_default_transition_time_id#
#define sl_btmesh_cmd_generic_client_init_default_transition_time_idValue:
0x081e0028
sl_btmesh_cmd_generic_client_init_power_on_off_id#
#define sl_btmesh_cmd_generic_client_init_power_on_off_idValue:
0x091e0028
sl_btmesh_cmd_generic_client_init_power_level_id#
#define sl_btmesh_cmd_generic_client_init_power_level_idValue:
0x0a1e0028
sl_btmesh_cmd_generic_client_init_battery_id#
#define sl_btmesh_cmd_generic_client_init_battery_idValue:
0x0b1e0028
sl_btmesh_cmd_generic_client_init_location_id#
#define sl_btmesh_cmd_generic_client_init_location_idValue:
0x0c1e0028
sl_btmesh_cmd_generic_client_init_property_id#
#define sl_btmesh_cmd_generic_client_init_property_idValue:
0x0d1e0028
sl_btmesh_cmd_generic_client_init_lightness_id#
#define sl_btmesh_cmd_generic_client_init_lightness_idValue:
0x0e1e0028
sl_btmesh_cmd_generic_client_init_ctl_id#
#define sl_btmesh_cmd_generic_client_init_ctl_idValue:
0x0f1e0028
sl_btmesh_cmd_generic_client_init_hsl_id#
#define sl_btmesh_cmd_generic_client_init_hsl_idValue:
0x101e0028
sl_btmesh_rsp_generic_client_publish_id#
#define sl_btmesh_rsp_generic_client_publish_idValue:
0x021e0028
sl_btmesh_rsp_generic_client_get_params_id#
#define sl_btmesh_rsp_generic_client_get_params_idValue:
0x031e0028
sl_btmesh_rsp_generic_client_init_common_id#
#define sl_btmesh_rsp_generic_client_init_common_idValue:
0x051e0028
sl_btmesh_rsp_generic_client_init_on_off_id#
#define sl_btmesh_rsp_generic_client_init_on_off_idValue:
0x061e0028
sl_btmesh_rsp_generic_client_init_level_id#
#define sl_btmesh_rsp_generic_client_init_level_idValue:
0x071e0028
sl_btmesh_rsp_generic_client_init_default_transition_time_id#
#define sl_btmesh_rsp_generic_client_init_default_transition_time_idValue:
0x081e0028
sl_btmesh_rsp_generic_client_init_power_on_off_id#
#define sl_btmesh_rsp_generic_client_init_power_on_off_idValue:
0x091e0028
sl_btmesh_rsp_generic_client_init_power_level_id#
#define sl_btmesh_rsp_generic_client_init_power_level_idValue:
0x0a1e0028
sl_btmesh_rsp_generic_client_init_battery_id#
#define sl_btmesh_rsp_generic_client_init_battery_idValue:
0x0b1e0028
sl_btmesh_rsp_generic_client_init_location_id#
#define sl_btmesh_rsp_generic_client_init_location_idValue:
0x0c1e0028
sl_btmesh_rsp_generic_client_init_property_id#
#define sl_btmesh_rsp_generic_client_init_property_idValue:
0x0d1e0028
sl_btmesh_rsp_generic_client_init_lightness_id#
#define sl_btmesh_rsp_generic_client_init_lightness_idValue:
0x0e1e0028
sl_btmesh_rsp_generic_client_init_ctl_id#
#define sl_btmesh_rsp_generic_client_init_ctl_idValue:
0x0f1e0028
sl_btmesh_rsp_generic_client_init_hsl_id#
#define sl_btmesh_rsp_generic_client_init_hsl_idValue:
0x101e0028