sl_btmesh_evt_generic_client_server_status#
Status report sent by a server model.
This may be generated either because of a response to a get or set request was received by the client model or because the client model received a spontaneously generated status indication sent to an address the model was subscribed to.
Modules#
sl_btmesh_evt_generic_client_server_status_s
Typedefs#
Macros#
#define
Identifier of the server_status event.
Typedef Documentation#
sl_btmesh_evt_generic_client_server_status_t#
typedef struct sl_btmesh_evt_generic_client_server_status_s sl_btmesh_evt_generic_client_server_status_t
Definition at line
5396
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_generic_client_server_status_id#
#define sl_btmesh_evt_generic_client_server_status_idValue:
0x001e00a8
Identifier of the server_status event.
Definition at line
5365
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h