Bluetooth Mesh On-demand Private Proxy Client Model#

Bluetooth Mesh On-demand Private Proxy Client Model.

The On-Demand Private Proxy Client model is used to configure a node to advertise with Private Network Identity

Modules#

sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status

Functions#

sl_status_t
sl_btmesh_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy(uint16_t enc_netkey_index, uint16_t server_address, uint32_t *handle)
sl_status_t
sl_btmesh_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy(uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t *handle)

Macros#

#define
sl_btmesh_cmd_on_demand_private_proxy_client_init_id 0x01680028
#define
sl_btmesh_cmd_on_demand_private_proxy_client_deinit_id 0x02680028
#define
sl_btmesh_cmd_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy_id 0x03680028
#define
sl_btmesh_cmd_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy_id 0x04680028
#define
sl_btmesh_rsp_on_demand_private_proxy_client_init_id 0x01680028
#define
sl_btmesh_rsp_on_demand_private_proxy_client_deinit_id 0x02680028
#define
sl_btmesh_rsp_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy_id 0x03680028
#define
sl_btmesh_rsp_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy_id 0x04680028

Function Documentation#

sl_btmesh_on_demand_private_proxy_client_init#

sl_status_t sl_btmesh_on_demand_private_proxy_client_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize the On-Demand Private Proxy Client model

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_on_demand_private_proxy_client_deinit#

sl_status_t sl_btmesh_on_demand_private_proxy_client_deinit (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Deinitialize the On-Demand Private Proxy Client model

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy#

sl_status_t sl_btmesh_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint32_t *[out]handle

Request handle

Get node On-Demand Private GATT proxy state.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_btmesh_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy#

sl_status_t sl_btmesh_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint8_t[in]value

On-Demand Private GATT proxy value to set. Valid values are:

  • 0: Advertising with Private Network Identity type cannot be enabled on demand

  • 1: Advertising interval for Private Network Identity in seconds

uint32_t *[out]handle

Request handle

Set node On-Demand Private GATT proxy state.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events