Bluetooth Mesh Key migration#

Bluetooth Mesh Key migration.

These commands are meant for migration from older releases to 3.2 and later releases.

Functions#

Function Documentation#

sl_btmesh_migration_migrate_keys#

sl_status_t sl_btmesh_migration_migrate_keys (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Ugrade keys from pre 3.2 release. Must be executed prior to to node or Provisioner initialization.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_migration_migrate_ddb#

sl_status_t sl_btmesh_migration_migrate_ddb (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Ugrade Device Database from pre 3.2 release. This command must be executed prior to provisioner initialization. Command may not be issued twice.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_btmesh_cmd_migration_migrate_keys_id#

#define sl_btmesh_cmd_migration_migrate_keys_id
Value:
0x01600028

sl_btmesh_cmd_migration_migrate_ddb_id#

#define sl_btmesh_cmd_migration_migrate_ddb_id
Value:
0x02600028

sl_btmesh_rsp_migration_migrate_keys_id#

#define sl_btmesh_rsp_migration_migrate_keys_id
Value:
0x01600028

sl_btmesh_rsp_migration_migrate_ddb_id#

#define sl_btmesh_rsp_migration_migrate_ddb_id
Value:
0x02600028