You are viewing documentation for version: 2.4 | 3.5 (latest) | Version History
- Global EMBER_MAX_ENDPOINT
- The maximum allowed endpoint value.
- Global EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH
- The maximum length in bytes of the application payload for a secured message. This define has been deprecated, you should use the emberGetMaximumPayloadLength API instead.
- Global emberIncomingBeaconHandler (EmberPanId panId, EmberNodeId nodeId, int8_t rssi, bool permitJoining, uint8_t payloadLength, uint8_t *payload)
- This stack handler has been deprecated and will be removed in a future release. The application should implement emberIncomingBeaconExtendedHandler instead.
- Global emberMacSetAllocateAddressFlag (bool allocateAddress)
- Configures the "allocate address" flag in the association request command for nodes joining as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE. This flag should be set if the device wishes to obtain a random 16-bit address from the coordinator. If cleared, the coordinator will not assign a 16-bit address to the device.