Ota Unicast Bootloader Client Plugin
Functions |
|
| bool | emberAfPluginOtaUnicastBootloaderClientNewIncomingImageCallback ( EmberNodeId serverId, uint8_t imageTag) |
|
A callback invoked by the OTA Unicast Client plugin when the client starts receiving a new image. The application can choose to start receiving the image or ignore(refuse) it. If the application chooses to receive the image, other images sent out by another server are ignored until the client completes this download.
More...
|
|
| void | emberAfPluginOtaUnicastBootloaderClientIncomingImageSegmentCallback ( EmberNodeId serverId, uint32_t startIndex, uint32_t endIndex, uint8_t imageTag, uint8_t *imageSegment) |
|
A callback invoked by the OTA Unicast Bootloader Client plugin when an image segment that is part of an image the application chose to download was received.
More...
|
|
| void | emberAfPluginOtaUnicastBootloaderClientImageDownloadCompleteCallback ( EmberAfOtaUnicastBootloaderStatus status, uint8_t imageTag, uint32_t imageSize) |
|
A callback invoked by the OTA Bootloader Client plugin to indicate that an image download has completed.
More...
|
|
| EmberAfOtaUnicastBootloaderStatus | emberAfPluginOtaUnicastBootloaderClientAbortImageDownload (uint8_t imageTag, uint8_t applicationErrorStatus) |
|
An API for aborting an ongoing image download process.
More...
|
|
| bool | emberAfPluginOtaUnicastBootloaderClientIncomingRequestBootloadCallback ( EmberNodeId serverId, uint8_t imageTag, uint32_t bootloadDelayMs, uint8_t *applicationStatus) |
|
A callback invoked by the OTA Unicast Bootloader Client plugin to indicate that an OTA Unicast Bootloader Server has requested to perform a bootload operation at a certain point in time in the future.
More...
|
|
Detailed Description
See
ota-unicast-bootloader-client.h
for source code.
Function Documentation
| EmberAfOtaUnicastBootloaderStatus emberAfPluginOtaUnicastBootloaderClientAbortImageDownload | ( | uint8_t |
imageTag,
|
| uint8_t |
applicationErrorStatus
|
||
| ) |
An API for aborting an ongoing image download process.
- Parameters
-
imageTagA 1-byte tag that identifies the image the client should no longer download. applicationErrorStatusA 1-byte error code that shall be reported to the server.
- Returns
-
An
EmberAfOtaUnicastBootloaderStatus
value of:
- EMBER_OTA_UNICAST_BOOTLOADER_STATUS_SUCCESS If the ongoing image download process was successfully aborted.
- EMBER_OTA_UNICAST_BOOTLOADER_STATUS_INVALID_CALL If the client was not currently involved in an image download process or it was currently downloading an image with a different tag.
| void emberAfPluginOtaUnicastBootloaderClientImageDownloadCompleteCallback | ( | EmberAfOtaUnicastBootloaderStatus |
status,
|
| uint8_t |
imageTag,
|
||
| uint32_t |
imageSize
|
||
| ) |
A callback invoked by the OTA Bootloader Client plugin to indicate that an image download has completed.
- Parameters
-
statusAn EmberAfOtaUnicastBootloaderStatus value of: - EMBER_OTA_UNICAST_BOOTLOADER_STATUS_SUCCESS indicating that the full image corresponding to the passed tag has been received. If this is the case, the client previously handed all the image segments to the application using the emberAfPluginOtaUnicastBootloaderClientIncomingImageSegmentCallback() callback.
- EMBER_OTA_UNICAST_BOOTLOADER_STATUS_FAILED indicating that the client failed to fully download the image and the download process was terminated.
- EMBER_OTA_UNICAST_BOOTLOADER_STATUS_TIMEOUT indicating that the client timed out waiting for a message from the server.
- EMBER_OTA_UNICAST_BOOTLOADER_STATUS_ABORTED indicating that the application aborted the ongoing image download process as result of calling the API emberAfPluginOtaUnicastBootloaderClientAbortImageDownload() .
imageTagA 1-byte tag of the image this callback refers to. imageSizeThe total size of the downloaded image in bytes. This parameter is meaningful only in case the status parameter is set to EMBER_OTA_UNICAST_BOOTLOADER_STATUS_SUCCESS .
| void emberAfPluginOtaUnicastBootloaderClientIncomingImageSegmentCallback | ( | EmberNodeId |
serverId,
|
| uint32_t |
startIndex,
|
||
| uint32_t |
endIndex,
|
||
| uint8_t |
imageTag,
|
||
| uint8_t * |
imageSegment
|
||
| ) |
A callback invoked by the OTA Unicast Bootloader Client plugin when an image segment that is part of an image the application chose to download was received.
- Parameters
-
serverIdThe node ID of the server that initiated the new image distribution process. startIndexThe index of the first byte of the passed segment. endIndexThe index of the last byte of the passed segment. imageTagA 1-byte tag of the image the passed segment belongs to. imageSegmentAn array containing the image segment.
| bool emberAfPluginOtaUnicastBootloaderClientIncomingRequestBootloadCallback | ( | EmberNodeId |
serverId,
|
| uint8_t |
imageTag,
|
||
| uint32_t |
bootloadDelayMs,
|
||
| uint8_t * |
applicationStatus
|
||
| ) |
A callback invoked by the OTA Unicast Bootloader Client plugin to indicate that an OTA Unicast Bootloader Server has requested to perform a bootload operation at a certain point in time in the future.
- Parameters
-
serverIdThe ID of the server the request came from. imageTagA 1-byte tag of the image this callback refers to. bootloadDelayMsThe delay in milliseconds after which the client has been requested to perform a bootload operation. applicationStatusA 1-byte status set by the client application that shall be reported to the server.
- Returns
- TRUE if the application accepted the request of bootloading the specified image at the requested time, FALSE otherwise.
| bool emberAfPluginOtaUnicastBootloaderClientNewIncomingImageCallback | ( | EmberNodeId |
serverId,
|
| uint8_t |
imageTag
|
||
| ) |
A callback invoked by the OTA Unicast Client plugin when the client starts receiving a new image. The application can choose to start receiving the image or ignore(refuse) it. If the application chooses to receive the image, other images sent out by another server are ignored until the client completes this download.
- Parameters
-
serverIdThe node ID of the server that initiated the new image distribution process. imageTagA 1-byte tag that identifies the incoming image.